Bluetooth LE Version 11.0.1 - Release Notes (Mar 25, 2026)#

Silicon Labs is a leading vendor in Bluetooth hardware and software technologies, used in products such as sports and fitness, consumer electronics, beacons, and smart home applications. The core SDK is an advanced Bluetooth 6.1-compliant stack that provides all of the core functionality along with multiple API to simplify development. The core functionality offers both standalone mode, allowing a developer to create and run their application directly on the SoC, or NCP mode, allowing for the use of an external host MCU.

Click here for earlier releases.

Release Summary#

Release Item Version Release Date Release Notes Key Features API Changes Bug Fixes Chip Enablement
Example and Middleware 11.0.1 Mar 25, 2026 Release Notes Channel Sounding: added support for max_procedure_count=1 in Real Time Fast mode. None Targeted quality improvements and bug fixes. None
Host Stack 11.0.1 Mar 25, 2026 Release Notes None None Targeted quality improvements and bug fixes. N/A
Controller 11.0.1 Mar 25, 2026 Release Notes None None Targeted quality improvements and bug fixes. N/A
802.15.4 Mesh + BLE Multiprotocol 11.0.1 Mar 25, 2026

Release Notes

Per-protocol TX power control in CMP applications. sl_802154_radio_set_scheduler_priorities() removed. Targeted quality improvements and bug fixes. None

Impact of Release Changes#

Impact Statements | Migration Guide

Impact Statements#

None.

Using This Release#

What's in the Release? | Compatible Software | Installation and Use | Help and Feedback

What's in the Release?#

Compatible Software#

Software Compatible Version or Variant
Simplicity SDK 2025.12.2
Simplicity Studio Any version that is compatible to Simplicity SDK 2025.12
Simplicity Commander provided with Simplicity Studio
GCC (The GNU Compiler Collection) 12.2.1 (provided with Simplicity Studio)
IAR Embedded Workbench for ARM (IAR-EWARM) 9.40.1

Installation and Use#

To run your first demo, see our Getting Started Guides.

To kick start your development, see our Developer's Guide.

For information about Secure Vault Integration, see Secure Vault.

To review Security and Software Advisory notifications and manage your notification preferences:

  1. Go to https://community.silabs.com/.

  2. Log in with your account credentials.

  3. Click your profile icon in the upper-right corner of the page.

  4. Select Notifications from the dropdown menu.

  5. In the Notifications section, go to the My Product Notifications tab to review historical Security and Software Advisory notifications

  6. To manage your preferences, use the Manage Notifications tab to customize which product updates and advisories you receive.

To learn more about the software in this release, dive into our online documentation.

Help and Feedback#

SDK Release and Maintenance Policy#

See our SDK Release and Maintenance Policy.