You are viewing documentation for version: 2.10 | Version History
Device Firmware Upgrade (dfu)
These commands and events are related to controlling firmware update over the configured host interface and are available only when the device has been booted into DFU mode.
The DFU process:
- Boot device to DFU mode with
DFU reset command
- Wait for
DFU boot event
- Send command
Flash Set Address to start the firmware update
- Upload the firmware with
Flash Upload commands until all the data has been uploaded
- Send
Flash Upload Finish when all the data has been uploaded
- Finalize the DFU firmware update with
Reset command.
DFU mode is using UART baudrate from hardware configuration of firmware. Default baudrate 115200 is used if firmware is missing or firmware content does not match with CRC checksum.
dfu commands
dfu_flash_set_address
After re-booting the local device into DFU mode, this command can be used to define the starting address on the flash to where the new firmware will be written in.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x01 |
method |
Message ID |
4-7 |
uint32 |
address |
The offset in the flash where the new firmware is uploaded to. Always use the value 0x00000000. |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x01 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_dfu_flash_set_address_rsp_t *gecko_cmd_dfu_flash_set_address(uint32 address);
/* Response id */
gecko_rsp_dfu_flash_set_address_id
/* Response structure */
struct gecko_msg_dfu_flash_set_address_rsp_t
{
uint16 result
}
dfu_flash_upload
This command can be used to upload the whole firmware image file into the Bluetooth device. The passed data length must be a multiple of 4 bytes. As the BGAPI command payload size is limited, multiple commands need to be issued one after the other
until the whole .bin firmware image file is uploaded to the device. The next address of the flash sector in memory to write to is automatically updated by the bootloader after each individual command.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x02 |
method |
Message ID |
4 |
uint8array |
data |
An array of data which will be written onto the flash. |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x02 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_dfu_flash_upload_rsp_t *gecko_cmd_dfu_flash_upload(uint8 data_len, const uint8 *data_data);
/* Response id */
gecko_rsp_dfu_flash_upload_id
/* Response structure */
struct gecko_msg_dfu_flash_upload_rsp_t
{
uint16 result
}
dfu_flash_upload_finish
This command can be used to tell to the device that the DFU file has been fully uploaded. To return the device back to normal mode the command
DFU Reset must be issued next.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x00 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x03 |
method |
Message ID |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x03 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_dfu_flash_upload_finish_rsp_t *gecko_cmd_dfu_flash_upload_finish();
/* Response id */
gecko_rsp_dfu_flash_upload_finish_id
/* Response structure */
struct gecko_msg_dfu_flash_upload_finish_rsp_t
{
uint16 result
}
dfu_reset
This command can be used to reset the system. This command does not have a response, but it triggers one of the boot events (normal reset or boot to DFU mode) after re-boot.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x00 |
method |
Message ID |
4 |
uint8 |
dfu |
Boot mode:
-
0: Normal reset
-
1: Boot to UART DFU mode
-
2: Boot to OTA DFU mode
|
Command does not have response
API
/* Function */
void *gecko_cmd_dfu_reset(uint8 dfu);
/* Command does not have response */
Events generated
Event |
Description |
system_boot
|
Sent after the device has booted into normal mode |
dfu_boot
|
Sent after the device has booted into UART DFU mode |
dfu events
dfu_boot
This event indicates that the device booted into DFU mode, and is now ready to receive commands related to device firmware upgade (DFU).
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x00 |
method |
Message ID |
4-7 |
uint32 |
version |
The version of the bootloader |
API
/* event id*/
gecko_evt_dfu_boot_id
/* event structure*/
struct gecko_msg_dfu_boot_evt_t
{
uint32 version
}
dfu_boot_failure
This event indicates that there has been error in bootloader, which prevents the device from booting.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x00 |
class |
Message class:Device Firmware Upgrade |
3 |
0x01 |
method |
Message ID |
4-5 |
uint16 |
reason |
The reason for boot failure, refer to the
Error codes
|
API
/* event id*/
gecko_evt_dfu_boot_failure_id
/* event structure*/
struct gecko_msg_dfu_boot_failure_evt_t
{
uint16 reason
}