Silicon Labs
bluetooth/2.11/bluetooth-api/endpoint
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
    Results 1-5 of 5 for bluetooth/2.11/bluetooth-api/endpoint in 0.16 seconds
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... get system.safemode.status faults_print faults_reset faults_print reboot ... file_delete
    ProductWireless Resource TypeSoftware API documentation
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    More. gos_result_t gos_cmd_issue_return_uint32 (uint32_t *uint32_ptr, const char *fmt,.) ... Issue Gecko OS command, store string result in buffer. ... fmt Formatted Gecko OS command Returns
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    Gecko OS writes the file to extended flash or bulk flash, depending on the location ... , file version defaults to 1.0.0 . -t <type> t ype: specify file type as integer or hex string 2 .
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    Return status is as follows: Status Description ... os pins can only use the strong drive strength. ... (This status is returned if i2cm_sda and i2cm_scl have not been assigned to a pin via ...
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for bluetooth/2.11/bluetooth-api/endpoint