You are viewing documentation for version: 2.12 | 3.0 (latest) | Version History
Coexistence interface (coex)
Coexistence BGAPI class. Coexistence interface is enabled and initialized with gecko_initCoexHAL() function.
coex commands
coex_get_counters
This command is used to read coexistence statistic counters from the device. Response contains the list of uint32 type counter values. Counters in the list are in following order: low priority requested, high priority requested, low priority denied, high priority denied, low priority tx aborted, high priority tx aborted.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x20 |
class |
Message class:Coexistence interface |
3 |
0x01 |
method |
Message ID |
4 |
uint8 |
reset |
Reset counter values |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0x20 |
class |
Message class:Coexistence interface |
3 |
0x01 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
6 |
uint8array |
counters |
Variable length byte array. The first byte defines the length of the data that
follows, 0 - 255 bytes. |
API
/* Function */
struct gecko_msg_coex_get_counters_rsp_t *gecko_cmd_coex_get_counters(uint8 reset);
/* Response id */
gecko_rsp_coex_get_counters_id
/* Response structure */
struct gecko_msg_coex_get_counters_rsp_t
{
uint16 result,
uint8array counters
}
coex_set_options
This command is used to configure coexistence options at runtime.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x08 |
lolen |
Minimum payload length |
2 |
0x20 |
class |
Message class:Coexistence interface |
3 |
0x00 |
method |
Message ID |
4-7 |
uint32 |
mask |
Mask defines which coexistence options are changed. |
8-11 |
uint32 |
options |
Value of options to be changed. This parameter is used together with mask parameter. |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x20 |
class |
Message class:Coexistence interface |
3 |
0x00 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_coex_set_options_rsp_t *gecko_cmd_coex_set_options(uint32 mask, uint32 options);
/* Response id */
gecko_rsp_coex_set_options_id
/* Response structure */
struct gecko_msg_coex_set_options_rsp_t
{
uint16 result
}
coex enumerations
coex_option
Coexistence configuration options
Enumerations
Value |
Name |
Description |
256 |
coex_option_enable |
Enable coexistence feature |
1024 |
coex_option_tx_abort |
Abort transmission if grant is denied |
2048 |
coex_option_high_priority |
Enable priority signal |