You are viewing documentation for version: 2.12 | 3.3 (latest) | Version History
CTE Receiver (cte_receiver)
Commands and events in this class can be used to manage Constant Tone Extension (CTE) receiving.
CTE feature is only supported by specific devices. Commands from this class will return bg_err_not_supported on devices that do not support CTE.
cte_receiver commands
cte_receiver_clear_dtm_parameters
This command can be used to clear CTE related parameters that were previously set for LE receiver test. Default values will be restored for these parameters.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x00 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x06 |
method |
Message ID |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x06 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_cte_receiver_clear_dtm_parameters_rsp_t *gecko_cmd_cte_receiver_clear_dtm_parameters();
/* Response id */
gecko_rsp_cte_receiver_clear_dtm_parameters_id
/* Response structure */
struct gecko_msg_cte_receiver_clear_dtm_parameters_rsp_t
{
uint16 result
}
cte_receiver_set_dtm_parameters
This command can be used to set CTE related parameters of LE receiver test.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x05 |
method |
Message ID |
4 |
uint8 |
cte_length |
Expected length of the Constant Tone Extension in 8 us units |
5 |
uint8 |
cte_type |
Expected CTE type
- 0: Expect AoA CTE
- 1: Expect AoD CTE with 1 us slots
- 2: Expect AoD CTE with 2 us slots
|
6 |
uint8 |
slot_durations |
Slot durations
- 1: Switching and sampling slots are 1 us each
- 2: Switching and sampling slots are 2 us each
|
7 |
uint8array |
switching_pattern |
Antenna switching pattern |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x05 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_cte_receiver_set_dtm_parameters_rsp_t *gecko_cmd_cte_receiver_set_dtm_parameters(uint8 cte_length, uint8 cte_type, uint8 slot_durations, uint8 switching_pattern_len, const uint8 *switching_pattern_data);
/* Response id */
gecko_rsp_cte_receiver_set_dtm_parameters_id
/* Response structure */
struct gecko_msg_cte_receiver_set_dtm_parameters_rsp_t
{
uint16 result
}
cte_receiver_start_iq_sampling
This command can be used to start IQ samplings on a connection.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x07 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x01 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
interval |
Measurement interval
- 0: No interval. The request is initiated only once.
- Other values N: Initiate the request every N-th connection events
|
7 |
uint8 |
cte_length |
Minimum length of the CTE being requested in 8 us units |
8 |
uint8 |
cte_type |
Requested CTE type
- 0: AoA CTE
- 1: AoD CTE with 1 us slots
- 2: AoD CTE with 2 us slots
|
9 |
uint8 |
slot_durations |
Slot durations
- 1: Switching and sampling slots are 1 us each
- 2: Switching and sampling slots are 2 us each
|
10 |
uint8array |
switching_pattern |
Antenna switching pattern |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x01 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_cte_receiver_start_iq_sampling_rsp_t *gecko_cmd_cte_receiver_start_iq_sampling(uint8 connection, uint16 interval, uint8 cte_length, uint8 cte_type, uint8 slot_durations, uint8 switching_pattern_len, const uint8 *switching_pattern_data);
/* Response id */
gecko_rsp_cte_receiver_start_iq_sampling_id
/* Response structure */
struct gecko_msg_cte_receiver_start_iq_sampling_rsp_t
{
uint16 result
}
Events generated
cte_receiver_stop_iq_sampling
This command can be used to stop the IQ sampling on a connection.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x02 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x02 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_cte_receiver_stop_iq_sampling_rsp_t *gecko_cmd_cte_receiver_stop_iq_sampling(uint8 connection);
/* Response id */
gecko_rsp_cte_receiver_stop_iq_sampling_id
/* Response structure */
struct gecko_msg_cte_receiver_stop_iq_sampling_rsp_t
{
uint16 result
}
cte_receiver events
cte_receiver_iq_report
IQ samples report from connection or connectionless CTE packets.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x0d |
lolen |
Minimum payload length |
2 |
0x45 |
class |
Message class:CTE Receiver |
3 |
0x00 |
method |
Message ID |
4-5 |
uint16 |
status |
Status of CTE IQ sampling |
6 |
uint8 |
packet_type |
CTE packet type
- 0: Connection
- 1: Connectionless
- 2: DTM. This value is possible only in some testing circumstances
|
7 |
uint8 |
handle |
Connection handle or periodic advertising synchronization handle |
8 |
uint8 |
phy |
The PHY on which the packet is received on a connection. Ingore this field for connectionless IQ reports.
|
9 |
uint8 |
channel |
The channel on which the CTE packet was received |
10 |
int8 |
rssi |
RSSI in the received CTE packet. Unit: dBm |
11 |
uint8 |
rssi_antenna_id |
The ID of the antenna on which RSSI was measured
|
12 |
uint8 |
cte_type |
The CTE type
- 0: AoA CTE response
- 1: AoD CTE response with 1us slots
- 2: AoD CTE response with 2us slots
|
13 |
uint8 |
slot_durations |
Slot durations
- 1: Switching and sampling slots are 1 us each
- 2: Switching and sampling slots are 2 us each
|
14-15 |
uint16 |
event_counter |
The event counter of the periodic advertising train or the connection
|
16 |
uint8array |
samples |
IQ samples in received CTE packet |
API
/* event id*/
gecko_evt_cte_receiver_iq_report_id
/* event structure*/
struct gecko_msg_cte_receiver_iq_report_evt_t
{
uint16 status,
uint8 packet_type,
uint8 handle,
uint8 phy,
uint8 channel,
int8 rssi,
uint8 rssi_antenna_id,
uint8 cte_type,
uint8 slot_durations,
uint16 event_counter,
uint8array samples
}