You are viewing documentation for version: 2.12 | 3.3 (latest) | Version History
Generic Attribute Profile (gatt)
The commands and events in this class can be used to browse and manage attributes in a remote GATT server.
gatt commands
gatt_discover_characteristics
This command can be used to discover all characteristics of the defined GATT service from a remote GATT database. This command generates a unique gatt_characteristic event for every discovered characteristic. Received gatt_procedure_completed event indicates that this GATT procedure has succesfully completed or failed with error.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x05 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x03 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-8 |
uint32 |
service |
GATT service handle This value is normally received from the gatt_service event.
|
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x03 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_discover_characteristics_rsp_t *gecko_cmd_gatt_discover_characteristics(uint8 connection, uint32 service);
/* Response id */
gecko_rsp_gatt_discover_characteristics_id
/* Response structure */
struct gecko_msg_gatt_discover_characteristics_rsp_t
{
uint16 result
}
Events generated
gatt_discover_characteristics_by_uuid
This command can be used to discover all the characteristics of the specified GATT service in a remote GATT database having the specified UUID. This command
generates a unique gatt_characteristic event for every discovered
characteristic having the specified UUID. Received gatt_procedure_completed event indicates that
this GATT procedure has successfully completed or failed with error.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x06 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x04 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-8 |
uint32 |
service |
GATT service handle This value is normally received from the gatt_service event.
|
9 |
uint8array |
uuid |
Characteristic UUID |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x04 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_discover_characteristics_by_uuid_rsp_t *gecko_cmd_gatt_discover_characteristics_by_uuid(uint8 connection, uint32 service, uint8 uuid_len, const uint8 *uuid_data);
/* Response id */
gecko_rsp_gatt_discover_characteristics_by_uuid_id
/* Response structure */
struct gecko_msg_gatt_discover_characteristics_by_uuid_rsp_t
{
uint16 result
}
Events generated
gatt_discover_descriptors
This command can be used to discover all the descriptors of the specified remote GATT characteristics in a remote GATT database. This command generates a unique gatt_descriptor event for every discovered descriptor. Received gatt_procedure_completed event indicates that this GATT procedure has succesfully completed or failed with error.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x06 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x06 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_discover_descriptors_rsp_t *gecko_cmd_gatt_discover_descriptors(uint8 connection, uint16 characteristic);
/* Response id */
gecko_rsp_gatt_discover_descriptors_id
/* Response structure */
struct gecko_msg_gatt_discover_descriptors_rsp_t
{
uint16 result
}
Events generated
gatt_discover_primary_services
This command can be used to discover all the primary services of a remote GATT database. This command generates a unique gatt_service event for
every discovered primary service. Received gatt_procedure_completed event indicates that this GATT procedure
has successfully completed or failed with error.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x01 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x01 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_discover_primary_services_rsp_t *gecko_cmd_gatt_discover_primary_services(uint8 connection);
/* Response id */
gecko_rsp_gatt_discover_primary_services_id
/* Response structure */
struct gecko_msg_gatt_discover_primary_services_rsp_t
{
uint16 result
}
Events generated
gatt_discover_primary_services_by_uuid
This command can be used to discover primary services with the specified UUID in a remote GATT database. This command generates unique gatt_service event for every discovered primary service. Received gatt_procedure_completed event indicates that this GATT procedure has succesfully completed or failed with error.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x02 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5 |
uint8array |
uuid |
Service UUID |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x02 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_discover_primary_services_by_uuid_rsp_t *gecko_cmd_gatt_discover_primary_services_by_uuid(uint8 connection, uint8 uuid_len, const uint8 *uuid_data);
/* Response id */
gecko_rsp_gatt_discover_primary_services_by_uuid_id
/* Response structure */
struct gecko_msg_gatt_discover_primary_services_by_uuid_rsp_t
{
uint16 result
}
Events generated
gatt_execute_characteristic_value_write
This command can be used to commit or cancel previously queued writes to a long characteristic of a remote GATT server.
Writes are sent to queue with prepare_characteristic_value_write command.
Content, offset and length of queued values are validated by this procedure. A received gatt_procedure_completed
event indicates that all data has been written successfully or that an error response has been received.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0c |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5 |
uint8 |
flags |
Unsigned 8-bit integer |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0c |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_execute_characteristic_value_write_rsp_t *gecko_cmd_gatt_execute_characteristic_value_write(uint8 connection, uint8 flags);
/* Response id */
gecko_rsp_gatt_execute_characteristic_value_write_id
/* Response structure */
struct gecko_msg_gatt_execute_characteristic_value_write_rsp_t
{
uint16 result
}
Events generated
gatt_find_included_services
This command can be used to find out if a service of a remote GATT database includes one or more other services. This command generates a unique gatt_service_completed event for each included service. This command generates a unique gatt_service event for every discovered service. Received gatt_procedure_completed event indicates that this GATT procedure has successfully completed or failed with error.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x05 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x10 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-8 |
uint32 |
service |
GATT service handle This value is normally received from the gatt_service event.
|
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x10 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_find_included_services_rsp_t *gecko_cmd_gatt_find_included_services(uint8 connection, uint32 service);
/* Response id */
gecko_rsp_gatt_find_included_services_id
/* Response structure */
struct gecko_msg_gatt_find_included_services_rsp_t
{
uint16 result
}
Events generated
gatt_prepare_characteristic_value_reliable_write
This command can be used to add a characteristic value to the write queue of a remote GATT server and verify if the value was correctly received by the server. Received gatt_procedure_completed event indicates that this GATT procedure has succesfully completed or failed with error. Specifically, error code 0x0194 (data_corrupted) will be returned if the value received from the GATT server's response failed to pass the reliable write verification. At most ATT_MTU - 5 amount of data can be sent once. Writes are executed or cancelled with the execute_characteristic_value_write command.
Whether the writes succeeded or not are indicated in the response of the execute_characteristic_value_write command.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x06 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x13 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
7-8 |
uint16 |
offset |
Offset of the characteristic value |
9 |
uint8array |
value |
Value to write into the specified characteristic of the remote GATT database |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x13 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
6-7 |
uint16 |
sent_len |
The length of data sent to the remote GATT server |
API
/* Function */
struct gecko_msg_gatt_prepare_characteristic_value_reliable_write_rsp_t *gecko_cmd_gatt_prepare_characteristic_value_reliable_write(uint8 connection, uint16 characteristic, uint16 offset, uint8 value_len, const uint8 *value_data);
/* Response id */
gecko_rsp_gatt_prepare_characteristic_value_reliable_write_id
/* Response structure */
struct gecko_msg_gatt_prepare_characteristic_value_reliable_write_rsp_t
{
uint16 result,
uint16 sent_len
}
Events generated
gatt_prepare_characteristic_value_write
This command can be used to add a characteristic value to the write queue of a remote GATT server.
This command can be used in cases where very long attributes need to be written, or a set of values needs to be written atomically. At most ATT_MTU - 5 amount of data can be sent once. Writes are executed or cancelled with the execute_characteristic_value_write command.
Whether the writes succeeded or not are indicated in the response of the execute_characteristic_value_write command.
In all cases where the amount of data to transfer fits into the BGAPI payload the command
gatt_write_characteristic_value is recommended for writing long values since it transparently
performs the prepare_write and execute_write commands.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x06 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0b |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
7-8 |
uint16 |
offset |
Offset of the characteristic value |
9 |
uint8array |
value |
Value to write into the specified characteristic of the remote GATT database |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0b |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
6-7 |
uint16 |
sent_len |
The length of data sent to the remote GATT server |
API
/* Function */
struct gecko_msg_gatt_prepare_characteristic_value_write_rsp_t *gecko_cmd_gatt_prepare_characteristic_value_write(uint8 connection, uint16 characteristic, uint16 offset, uint8 value_len, const uint8 *value_data);
/* Response id */
gecko_rsp_gatt_prepare_characteristic_value_write_id
/* Response structure */
struct gecko_msg_gatt_prepare_characteristic_value_write_rsp_t
{
uint16 result,
uint16 sent_len
}
Events generated
gatt_read_characteristic_value
This command can be used to read the value of a characteristic from a remote GATT database.
A single gatt_characteristic_value event is generated if the
characteristic value fits in one ATT PDU. Otherwise more than one
gatt_characteristic_value events are generated because the firmware will automatically use the "read long"
GATT procedure. A received gatt_procedure_completed event indicates
that all data has been read successfully or that an error response has been received.
Note that the GATT client does not verify if the requested atrribute is a characteristic value.
Thus before calling this command the application should make sure the attribute handle is for a characteristic
value in some means, for example, by performing characteristic discovery.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x07 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x07 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_read_characteristic_value_rsp_t *gecko_cmd_gatt_read_characteristic_value(uint8 connection, uint16 characteristic);
/* Response id */
gecko_rsp_gatt_read_characteristic_value_id
/* Response structure */
struct gecko_msg_gatt_read_characteristic_value_rsp_t
{
uint16 result
}
Events generated
gatt_read_characteristic_value_by_uuid
This command can be used to read the characteristic value of a service from a remote GATT database
by giving the UUID of the characteristic and the handle of the service containing this characteristic. A single
gatt_characteristic_value event is generated if the characteristic
value fits in one ATT PDU. Otherwise more than one
gatt_characteristic_value events are generated because the firmware will automatically use the "read long" GATT procedure.
A received gatt_procedure_completed event indicates that all data has been read successfully or that an error response has been received.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x06 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x08 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-8 |
uint32 |
service |
GATT service handle This value is normally received from the gatt_service event.
|
9 |
uint8array |
uuid |
Characteristic UUID |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x08 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_read_characteristic_value_by_uuid_rsp_t *gecko_cmd_gatt_read_characteristic_value_by_uuid(uint8 connection, uint32 service, uint8 uuid_len, const uint8 *uuid_data);
/* Response id */
gecko_rsp_gatt_read_characteristic_value_by_uuid_id
/* Response structure */
struct gecko_msg_gatt_read_characteristic_value_by_uuid_rsp_t
{
uint16 result
}
Events generated
gatt_read_characteristic_value_from_offset
This command can be used to read a partial characteristic value with specified offset and maximum length
from a remote GATT database. It is equivalent to
gatt_read_characteristic_value
if both the offset and maximum length parameters are 0.
A single gatt_characteristic_value event is generated
if the value to read fits in one ATT PDU. Otherwise more than one
gatt_characteristic_value events are generated because the firmware will automatically use the "read long"
GATT procedure. A received gatt_procedure_completed event indicates
that all data has been read successfully or that an error response has been received.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x07 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x12 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
7-8 |
uint16 |
offset |
Offset of the characteristic value |
9-10 |
uint16 |
maxlen |
Maximum bytes to read. If this parameter is 0 all characteristic value starting at given offset will be read.
|
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x12 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_read_characteristic_value_from_offset_rsp_t *gecko_cmd_gatt_read_characteristic_value_from_offset(uint8 connection, uint16 characteristic, uint16 offset, uint16 maxlen);
/* Response id */
gecko_rsp_gatt_read_characteristic_value_from_offset_id
/* Response structure */
struct gecko_msg_gatt_read_characteristic_value_from_offset_rsp_t
{
uint16 result
}
Events generated
gatt_read_descriptor_value
This command can be used to read the descriptor value of a characteristic in a remote GATT database. A single
gatt_descriptor_value event is generated if the descriptor value fits in one ATT PDU. Otherwise more than one gatt_descriptor_value events are generated because the firmware
will automatically use the "read long" GATT procedure. A received gatt_procedure_completed event indicates that all
data has been read successfully or that an error response has been received.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0e |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
descriptor |
GATT characteristic descriptor handle |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0e |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_read_descriptor_value_rsp_t *gecko_cmd_gatt_read_descriptor_value(uint8 connection, uint16 descriptor);
/* Response id */
gecko_rsp_gatt_read_descriptor_value_id
/* Response structure */
struct gecko_msg_gatt_read_descriptor_value_rsp_t
{
uint16 result
}
Events generated
gatt_read_multiple_characteristic_values
This command can be used to read the values of multiple characteristics from a remote GATT database at once.
The GATT server will return the values in one ATT PDU as the response. If the total set of values is greater than
(ATT_MTU - 1) bytes in length, only the first (ATT_MTU - 1) bytes are included. A single
gatt_characteristic_value event is generated, in which the
characteristic is set to 0 and the data in value parameter is a concatenation of characteristic values in the order
they were requested.
Received gatt_procedure_completed event indicates that this GATT procedure
has successfully completed or failed with error.
This command should be used only for characteristics values that have known fixed size, except the last one that could have variable length.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x11 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5 |
uint8array |
characteristic_list |
Little endian encoded uint16 list of characteristics to be read. |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x11 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_read_multiple_characteristic_values_rsp_t *gecko_cmd_gatt_read_multiple_characteristic_values(uint8 connection, uint8 characteristic_list_len, const uint8 *characteristic_list_data);
/* Response id */
gecko_rsp_gatt_read_multiple_characteristic_values_id
/* Response structure */
struct gecko_msg_gatt_read_multiple_characteristic_values_rsp_t
{
uint16 result
}
Events generated
gatt_send_characteristic_confirmation
This command must be used to send a characteristic confirmation to a remote GATT server after receiving an indication.
The gatt_characteristic_value_event carries the att_opcode containing handle_value_indication (0x1d) which reveals
that an indication has been received and this must be confirmed with this command. Confirmation needs to be sent within 30 seconds, otherwise the GATT transactions
between the client and the server are discontinued.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0d |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0d |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_send_characteristic_confirmation_rsp_t *gecko_cmd_gatt_send_characteristic_confirmation(uint8 connection);
/* Response id */
gecko_rsp_gatt_send_characteristic_confirmation_id
/* Response structure */
struct gecko_msg_gatt_send_characteristic_confirmation_rsp_t
{
uint16 result
}
gatt_set_characteristic_notification
This command can be used to enable or disable the notifications and indications being sent from a remote GATT server. This procedure discovers a
characteristic client configuration descriptor and writes the related configuration flags to a remote GATT database. A received gatt_procedure_completed event
indicates that this GATT procedure has successfully completed or that is has failed with an error.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x05 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
7 |
uint8 |
flags |
Characteristic client configuration flags |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x05 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_set_characteristic_notification_rsp_t *gecko_cmd_gatt_set_characteristic_notification(uint8 connection, uint16 characteristic, uint8 flags);
/* Response id */
gecko_rsp_gatt_set_characteristic_notification_id
/* Response structure */
struct gecko_msg_gatt_set_characteristic_notification_rsp_t
{
uint16 result
}
Events generated
Event |
Description |
gatt_procedure_completed |
Procedure has been successfully completed or failed with error. |
gatt_characteristic_value |
If an indication or notification has been enabled for a characteristic, this event is triggered
whenever an indication or notification is sent by the remote GATT server. The triggering conditions on the GATT server side are defined by an
upper level, for example by a profile; so it is possible that no values are ever received, or that it may take time, depending on how the server is configured. |
gatt_set_max_mtu
This command can be used to set the maximum size of ATT Message Transfer Units (MTU).
Functionality is the same as gatt_server_set_max_mtu, and this setting applies to both GATT client and server.
If the given value is too large according to the maximum BGAPI payload size, the system will select the maximal possible
value as the maximum ATT_MTU. If maximum ATT_MTU is larger than 23, the GATT client in stack will automatically
send an MTU exchange request after a Bluetooth connection has been established.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x00 |
method |
Message ID |
4-5 |
uint16 |
max_mtu |
Maximum size of Message Transfer Units (MTU) allowedDefault: 247 |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x00 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
6-7 |
uint16 |
max_mtu |
The maximum ATT_MTU selected by the system if this command succeeded |
API
/* Function */
struct gecko_msg_gatt_set_max_mtu_rsp_t *gecko_cmd_gatt_set_max_mtu(uint16 max_mtu);
/* Response id */
gecko_rsp_gatt_set_max_mtu_id
/* Response structure */
struct gecko_msg_gatt_set_max_mtu_rsp_t
{
uint16 result,
uint16 max_mtu
}
gatt_write_characteristic_value
This command can be used to write the value of a characteristic in a remote GATT database. If the given value does not fit in one ATT PDU, "write long" GATT procedure is used automatically. Received
gatt_procedure_completed event indicates that all data has been written successfully or that an error response
has been received.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x09 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
7 |
uint8array |
value |
Characteristic value |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x09 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_write_characteristic_value_rsp_t *gecko_cmd_gatt_write_characteristic_value(uint8 connection, uint16 characteristic, uint8 value_len, const uint8 *value_data);
/* Response id */
gecko_rsp_gatt_write_characteristic_value_id
/* Response structure */
struct gecko_msg_gatt_write_characteristic_value_rsp_t
{
uint16 result
}
Events generated
gatt_write_characteristic_value_without_response
This command can be used to write the value of a characteristic in a
remote GATT server. This command does not generate any event. All failures on the server are ignored silently.
For example, if an error is generated in the remote GATT server and the given value is not written into database no error message will be reported to the local
GATT client. Note that this command cannot be used to write long values. At most ATT_MTU - 3 amount of data can be sent once.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0a |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
7 |
uint8array |
value |
Characteristic value |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0a |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
6-7 |
uint16 |
sent_len |
The length of data sent to the remote GATT server |
API
/* Function */
struct gecko_msg_gatt_write_characteristic_value_without_response_rsp_t *gecko_cmd_gatt_write_characteristic_value_without_response(uint8 connection, uint16 characteristic, uint8 value_len, const uint8 *value_data);
/* Response id */
gecko_rsp_gatt_write_characteristic_value_without_response_id
/* Response structure */
struct gecko_msg_gatt_write_characteristic_value_without_response_rsp_t
{
uint16 result,
uint16 sent_len
}
gatt_write_descriptor_value
This command can be used to write the value of a characteristic descriptor in a remote GATT database. If the given value does not fit in one ATT PDU, "write long" GATT procedure is used automatically. Received gatt_procedure_completed
event indicates that all data has been written succesfully or that an error response has been received.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0f |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
descriptor |
GATT characteristic descriptor handle |
7 |
uint8array |
value |
Descriptor value |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x0f |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* Function */
struct gecko_msg_gatt_write_descriptor_value_rsp_t *gecko_cmd_gatt_write_descriptor_value(uint8 connection, uint16 descriptor, uint8 value_len, const uint8 *value_data);
/* Response id */
gecko_rsp_gatt_write_descriptor_value_id
/* Response structure */
struct gecko_msg_gatt_write_descriptor_value_rsp_t
{
uint16 result
}
Events generated
gatt events
gatt_mtu_exchanged
This event indicates that an ATT_MTU exchange procedure has been completed. Parameter mtu describes new MTU size. MTU size 23 is used before this event is received.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x00 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
mtu |
Exchanged ATT_MTU |
API
/* event id*/
gecko_evt_gatt_mtu_exchanged_id
/* event structure*/
struct gecko_msg_gatt_mtu_exchanged_evt_t
{
uint8 connection,
uint16 mtu
}
gatt_service
This event indicates that a GATT service in the remote GATT database was discovered. This event is generated after issuing either the
gatt_discover_primary_services or
gatt_discover_primary_services_by_uuid command.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x06 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x01 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-8 |
uint32 |
service |
GATT service handle |
9 |
uint8array |
uuid |
Service UUID |
API
/* event id*/
gecko_evt_gatt_service_id
/* event structure*/
struct gecko_msg_gatt_service_evt_t
{
uint8 connection,
uint32 service,
uint8array uuid
}
gatt_characteristic
This event indicates that a GATT characteristic in the remote GATT database was discovered. This event is generated after issuing either the
gatt_discover_characteristics or gatt_discover_characteristics_by_uuid command.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x05 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x02 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle |
7 |
uint8 |
properties |
Characteristic properties |
8 |
uint8array |
uuid |
Characteristic UUID |
API
/* event id*/
gecko_evt_gatt_characteristic_id
/* event structure*/
struct gecko_msg_gatt_characteristic_evt_t
{
uint8 connection,
uint16 characteristic,
uint8 properties,
uint8array uuid
}
gatt_descriptor
This event indicates that a GATT characteristic descriptor in the remote GATT database was discovered. This event is generated after issuing the
gatt_discover_descriptors command.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x04 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x03 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
descriptor |
GATT characteristic descriptor handle |
7 |
uint8array |
uuid |
Descriptor UUID |
API
/* event id*/
gecko_evt_gatt_descriptor_id
/* event structure*/
struct gecko_msg_gatt_descriptor_evt_t
{
uint8 connection,
uint16 descriptor,
uint8array uuid
}
gatt_characteristic_value
This event indicates that the value of one or several characteristics in the remote GATT server was received. This event is triggered as a result of several commands: gatt_read_characteristic_value,
gatt_read_characteristic_value_from_offset,
gatt_read_characteristic_value_by_uuid,
gatt_read_multiple_characteristic_values; and when the remote GATT server sends indications or notifications after enabling notifications with gatt_set_characteristic_notification.
The parameter att_opcode reveals which type of GATT transaction triggered this event.
In particular, if the att_opcode type is handle_value_indication (0x1d), the application needs to confirm the indication with
gatt_send_characteristic_confirmation.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x07 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x04 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
characteristic |
GATT characteristic handle This value is normally received from the gatt_characteristic event.
|
7 |
uint8 |
att_opcode |
Attribute opcode which informs the GATT transaction used |
8-9 |
uint16 |
offset |
Value offset |
10 |
uint8array |
value |
Characteristic value |
API
/* event id*/
gecko_evt_gatt_characteristic_value_id
/* event structure*/
struct gecko_msg_gatt_characteristic_value_evt_t
{
uint8 connection,
uint16 characteristic,
uint8 att_opcode,
uint16 offset,
uint8array value
}
gatt_descriptor_value
This event indicates that the value of a descriptor in the remote GATT server was received. This event is generated by the
gatt_read_descriptor_value command.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x06 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x05 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
descriptor |
GATT characteristic descriptor handle |
7-8 |
uint16 |
offset |
Value offset |
9 |
uint8array |
value |
Descriptor value |
API
/* event id*/
gecko_evt_gatt_descriptor_value_id
/* event structure*/
struct gecko_msg_gatt_descriptor_value_evt_t
{
uint8 connection,
uint16 descriptor,
uint16 offset,
uint8array value
}
gatt_procedure_completed
This event indicates that the current GATT procedure has been completed successfully or that it has failed with an error. All GATT commands excluding
gatt_write_characteristic_value_without_response and
gatt_send_characteristic_confirmation will trigger this event, so the application must wait for this event before issuing another GATT command (excluding the
two aforementioned exceptions).
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0x09 |
class |
Message class:Generic Attribute Profile |
3 |
0x06 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error occurred
For other values refer to the Error codes
|
API
/* event id*/
gecko_evt_gatt_procedure_completed_id
/* event structure*/
struct gecko_msg_gatt_procedure_completed_evt_t
{
uint8 connection,
uint16 result
}
gatt enumerations
gatt_att_opcode
These values indicate which attribute request or response has caused the event.
Enumerations
Value |
Name |
Description |
8 |
gatt_read_by_type_request |
Read by type request |
9 |
gatt_read_by_type_response |
Read by type response |
10 |
gatt_read_request |
Read request |
11 |
gatt_read_response |
Read response |
12 |
gatt_read_blob_request |
Read blob request |
13 |
gatt_read_blob_response |
Read blob response |
14 |
gatt_read_multiple_request |
Read multiple request |
15 |
gatt_read_multiple_response |
Read multiple response |
18 |
gatt_write_request |
Write request |
19 |
gatt_write_response |
Write response |
82 |
gatt_write_command |
Write command |
22 |
gatt_prepare_write_request |
Prepare write request |
23 |
gatt_prepare_write_response |
Prepare write response |
24 |
gatt_execute_write_request |
Execute write request |
25 |
gatt_execute_write_response |
Execute write response |
27 |
gatt_handle_value_notification |
Notification |
29 |
gatt_handle_value_indication |
Indication |
gatt_client_config_flag
These values define whether the client is to receive notifications or indications from a remote GATT server.
Enumerations
Value |
Name |
Description |
0 |
gatt_disable |
Disable notifications and indications |
1 |
gatt_notification |
Notification |
2 |
gatt_indication |
Indication |
gatt_execute_write_flag
These values define whether the GATT server is to cancel all queued writes or commit all queued writes to a remote database.
Enumerations
Value |
Name |
Description |
0 |
gatt_cancel |
Cancel all queued writes |
1 |
gatt_commit |
Commit all queued writes |