Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ...
ProductWirelessResource TypeSoftware API documentation
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
Training ... You are viewing documentation for version: 4.4.4 Gecko Platform# Gecko Platform is the common foundation for the Gecko SDK Suite. Gecko Platform Components# Getting Started
Training ... Register ... Local regulatory bodies put limitations on how much power a radio equipment is allowed to radiate. ... The power limits discussed here are the absolute maximums.