2.33 µA 2.66 µA 2.75 µA ... Using LFXO instead of PLFRCO will reduce the current consumption. ... a new SoC - Empty application project with Bluetooth SDK using version 2.13.6 or newer.
// Bluetooth LE//Version 2.13 // Code Examples //Applications ... To keep the code as short and simple as possible, the features are minimal. ... The custom service is as minimal as possible.
// Bluetooth LE//Version 2.13 // Code Examples //Stack Features ... This example shows how advertising on the coded PHY works, as well how to establish a connection using the coded PHY.
You are viewing documentation for version: 2.13 Using Energy Modes with Bluetooth Stack# Introduction# ... This guide has a related code example here: Using energy modes with Bluetooth stack
2.4GHz Protocol Field Day RF Transfer of Power ... Bluetooth 5.2 Bluetooth mesh LPN Direction Finding ... Hardware Cryptographic Acceleration True Random Number Generator compliant with
Resource TypePresentations
Results 1-5 of 5 for bluetooth/2.13/code-examples/peripheral/using-hardware-timers