// Code Examples //Stack Features //Advertising & Scanning //Advertising and Scanning with LE Coded PHY ... One of the new features added in Bluetooth 5 is the LE coded PHY, which enables ...
//General //Advertising and Scanning //Bluetooth Advertising Data Basics You are viewing ... Bluetooth Core Specification - This is the golden reference, but not that easy to digest.
When creating an "SoC - Empty" project, the initial sleep current can be measured at around ... 1.Create a new SoC - Empty application project with Bluetooth SDK using version 2.13.6 or newer.
2.4GHz Protocol Field Day RF Transfer of Power ... on docs.silabs.com https://docs.silabs.com/bluetooth/latest/code-examples/stack-features/system-and-performance/waking-from-deep-sleep-using- ...
2. BLE-112: Using Manufacturer Specific Data ... Bluetooth 102 - Advertising Training Series ... of Bluetooth advertising packets are formatted and decoded using two basic examples – ...
ProductWirelessResource TypeWritten Materials
Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/adv-and-scanning/creating-an-eddystone-url-beacon