Silicon Labs
bluetooth/2.13/code-examples/stack-features/gatt-protocol/working-with-long-characteristic-values
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
      Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/gatt-protocol/working-with-long-characteristic-values in 0.19 seconds
      EFR32xG22-Power-Consumption-Optimization | Peripheral | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/.../efr32x-g22-power-consumption-optimizat...
      With temperature variations, PLFRCO(LFRCO in precision mode) will autonomously run frequent ... 1.Create a new SoC - Empty application project with Bluetooth SDK using version 2.13.6 or newer.
      Advertising and Scanning with LE Coded PHY | Advertising & Scanning | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/.../adv-and-scanning-with-le-coded-...
      // Bluetooth LE//Version 2.13 // Code Examples //Stack Features //Advertising & Scanning ... One of the new features added in Bluetooth 5 is the LE coded PHY, which enables longer range ...
      SPP (Serial Port Profile) over BLE | Applications | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/....
      // Bluetooth LE//Version 2.13 // ... with the command gatt_server_send_characteristic_notification are used. ... Call gatt_set_characteristic_notification to enable notifications for spp_data ...
      Tech Talks: Wake Bluetooth from Deep Sleep Using and RF Signal
      https://www.silabs.com/.../tech-talks-wake-bluetooth-from-deep-sleep-using-an-rf-signal....
      Long Range Connectivity using Proprietary RF Solution ... on docs.silabs.com https://docs.silabs.com/bluetooth/latest/code-examples/stack-features/system-and-performance/waking-from-deep-sleep ...
      Resource TypePresentations
      Implementing OTA Firmware Update in User Application | Firmware Upgrade | Bluetooth LE | v2.13 | Silicon Labs
      https://docs.silabs.com/.../implementing-ota-firmware-update-in-user-applicat...
      // Bluetooth LE//Version 2.13 // Code Examples //Stack Features //Firmware Upgrade ... Import the attached GATT database (gatt.xml) into the project. ... app.h gatt.xml Table of Contents
        Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/gatt-protocol/working-with-long-characteristic-values