Bluetooth functions in the 2.4 GHz frequency range. ... Channel map update procedure is part of the Bluetooth 4.0 specification. ... Bluetooth Low Energy has two channel selection algorithms.
Training ... // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... These values define the packet types in legacy and extended advertising. Functions# sl_status_t
// Bluetooth LE//Version 3.1 //General ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 dBm in those cases when AFH is not enabled (or AFH is enabled but ...
This Bluetooth advertising training reviews the basics of this fundamental Bluetooth LE operation, and introduces customizing your advertising ... Bluetooth 102 - Advertising Training Series
ProductWirelessResource TypeWritten Materials
Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/ncp/adding-watchdog-in-ncp-mode