In accordance with "AEM Accuracy and Performance" section from UG172, the AEM is capable of ... .Create a new SoC - Empty application project with Bluetooth SDK using version 2.13.6 or newer.
// Bluetooth LE//Version 2.13 // Code Examples //Stack Features //Advertising & Scanning ... In this new type of advertisement, the same three advertising channels are used but instead of ...
Data is received over the air by notifications (event gatt_characteristic_value). ... In this use case, types 0x06 and 0x07 that indicate incomplete/complete list of 128-bit service values are ...
2.4GHz Protocol Field Day RF Transfer of Power ... Manchester-coded Data DE ... In Legacy (Energy Detection) mode, EFR32xG22 RF Sense is fully compatible with the feature in Series 1 devices
You are viewing documentation for version: 2.13 Using Energy Modes with Bluetooth Stack# Introduction# ... In this mode, nearly everything is shut down and the current consumption is around ...
Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/persistent-storage/saving-arbitrary-data-in-ps-keys