// Code Examples //Applications ... With temperature variations, PLFRCO(LFRCO in precision mode) will autonomously run ... Using LFXO instead of PLFRCO will reduce the current consumption.
2.4GHz Protocol Field Day RF Transfer of Power ... docs.silabs.com https://docs.silabs.com/bluetooth/latest/code-examples/stack-features/system-and-performance/waking-from-deep-sleep-using-rf- ...
// Bluetooth LE//Version 2.13 // Code Examples //Stack Features //Advertising & Scanning ... One of the new features added in Bluetooth 5 is the LE coded PHY, which enables longer range ...
Energy Management Unit (EMU) ensures that only actively needed peripherals are running and consuming ... With sleep driver the EM2 Deep sleep mode can be disabled (/blocked) temporarily by ...
Training ... Register ... To keep the code as short and simple as possible, the features are minimal. ... For more details on power management, see Using Energy Modes with Bluetooth Stack.
Results 1-5 of 5 for bluetooth/2.13/code-examples/stack-features/system-and-performance/using-energy-modes-with-bluetooth-stack