You are viewing documentation for version: 2.13 This version works with Simplicity Studio 4 only | For the latest and prior versions see Version History.
Coexistence Interface (coex)
Coexistence BGAPI class. Coexistence interface is enabled and initialized with gecko_initCoexHAL() function.
coex commands
coex_get_counters
Read coexistence statistic counters from the device. Response contains the list of uint32 type counter values. Counters in the list are in following order: low priority requested, high priority requested, low priority denied, high priority denied, low-priority TX aborted, and high-priority TX aborted. Passing a non-zero value also resets counters.
C API
/* Function */
struct gecko_msg_coex_get_counters_rsp_t *gecko_cmd_coex_get_counters(uint8 reset);
/* Response id */
gecko_rsp_coex_get_counters_id
/* Response structure */
struct gecko_msg_coex_get_counters_rsp_t
{
uint16 result;
uint8array counters;
}
Command Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint8 |
reset |
Reset counters if parameter value is not zero. |
Response Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error has occurred
For other values see Error codes
|
uint8array |
counters |
Variable length byte array. The first byte defines the length of data that follows, 0 - 255 bytes. |
coex_set_directional_priority_pulse
Set Directional Priority Pulse Width
C API
/* Function */
struct gecko_msg_coex_set_directional_priority_pulse_rsp_t *gecko_cmd_coex_set_directional_priority_pulse(uint8 pulse);
/* Response id */
gecko_rsp_coex_set_directional_priority_pulse_id
/* Response structure */
struct gecko_msg_coex_set_directional_priority_pulse_rsp_t
{
uint16 result;
}
Command Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint8 |
pulse |
Directional priority pulse width in us |
Response Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error has occurred
For other values see Error codes
|
coex_set_options
Configure coexistence options at runtime.
C API
/* Function */
struct gecko_msg_coex_set_options_rsp_t *gecko_cmd_coex_set_options(uint32 mask, uint32 options);
/* Response id */
gecko_rsp_coex_set_options_id
/* Response structure */
struct gecko_msg_coex_set_options_rsp_t
{
uint16 result;
}
Command Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint32 |
mask |
Mask defines which coexistence options are changed. |
uint32 |
options |
Value of options to be changed. This parameter is used together with the mask parameter. |
Response Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error has occurred
For other values see Error codes
|
coex_set_parameters
Configure coexistence parameters.
C API
/* Function */
struct gecko_msg_coex_set_parameters_rsp_t *gecko_cmd_coex_set_parameters(uint8 priority, uint8 request, uint8 pwm_period, uint8 pwm_dutycycle);
/* Response id */
gecko_rsp_coex_set_parameters_id
/* Response structure */
struct gecko_msg_coex_set_parameters_rsp_t
{
uint16 result;
}
Command Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint8 |
priority |
Coexistence priority threshold. Coexistence priority is toggled if priority is below this value. |
uint8 |
request |
Coexistence request threshold. Coexistence request is toggled if priority is below this value. |
uint8 |
pwm_period |
PWM functionality period length in 1ms units |
uint8 |
pwm_dutycycle |
PWM functionality dutycycle in percentage |
Response Parameters (for BGAPI headers refer to link)
Type |
Name |
Description |
uint16 |
result |
Result code
- 0: success
- Non-zero: an error has occurred
For other values see Error codes
|
coex enumerations
coex_option
Coexistence configuration options
Enumerations
Value |
Name |
Description |
256 |
coex_option_enable |
Enable coexistence feature |
1024 |
coex_option_tx_abort |
Abort transmission if grant is denied |
2048 |
coex_option_high_priority |
Enable priority signal |