Using Blue Gecko Mobile App for OTA DFU
Introduction
This tutorial explains how to perform a Device Firmware Upgrade (DFU) with Bluetooth Over-The-Air (OTA) upgrade. Any chip that has OTA-upgrades enabled in their GATT profile can have an OTA upgrade. Most of the example applications provided in the Bluetooth SDK already have OTA support built into the code. In these examples, the DFU mode is triggered through the Silicon Labs OTA service that is included as part of the application’s GATT database. This can be checked and added in the BLE GATT Configurator in Simplicity Studio.
For tutorial purposes, the SOC - Empty
SDK example application will be upgraded to the SoC - Smart Phone App
example application.
Because the smart phone example has the Health Thermometer service for visual feedback, users can easily check that the functionality of the user application has changed.
Requirements:
- Wireless Starter Kit and Bluetooth-capable radio board
- Simplicity Studio
- Android or iOS mobile device
First Steps
Connect the kit to your computer and select it in Simplicity Studio.
Run the
SOC - Empty
demo from Simplicity Studio Launcher.Create
SoC - Smart Phone App
Software Examples project.Build the
SoC - Smart Phone
project and runcreate_bl_files.bat/sh
script from the smart phone project tree. This creates a folder namedoutput_gbl
under your project. There are three.gbl
upgrade image files in this folder:application.gbl
: user application (including full Bluetooth stack)apploader.gbl
: AppLoader (including minimal Bluetooth stack)full.gbl
: For UART DFU, not needed in this example. Starting from SDK 2.7.0, the user application also includes the Bluetooth stack and therefore the Bluetooth stack can be updated without a full update. A full update is needed only if the AppLoader needs to be updated. See AN1086 for more details.
Transfer the
.gbl
files to your smart phone so the mobile app can find them.- Android users can use any transfer method e.g., Dropbox. They need to navigate to SiliconLabs_BGApp/OTAFiles directory in their phone's file system and create a new subfolder for storing the
.gbl
files. This is where the Blue Gecko App can locate them. - iOS users can upload the files to iCloud. The app will prompt you to bring the files from iCloud.
- Android users can use any transfer method e.g., Dropbox. They need to navigate to SiliconLabs_BGApp/OTAFiles directory in their phone's file system and create a new subfolder for storing the
Launch the Blue Gecko mobile app.
In the Blue Gecko App
Once in the app,
Go to the
Bluetooth Browser
and find and connect to your kit (default name "Empty Example").Open the pop-up menu in the upper right corner and select
OTA
.Select
Partial OTA
and look for your newly created folder in theFolder
drop down menu. iOS users can select from iCloud at this stage.Once you have selected the folder, select your
.gbl
image from theApp
drop down. Use theapplication.gbl
image.Finally, press
OTA
and your upgrade should start.After the OTA process has finished, verify that the kit is now running the
SoC - Smart Phone App
example. You can find the kit in theBluetooth Browser
with a new name, such as "BGXXXXX". The name is also shown on the LCD.
Note:
To enable the Bluetooth OTA upgrade, the target device must be programmed with the Gecko Bootloader that is configured as an Internal Storage Bootloader. This is an application bootloader, which requires that the new firmware image acquisition is managed by the application. Running the "Demos" in Simplicity Studio will include the bootloader and user application. However, flashing a "Software Example" does not. If your OTA upload stops at 0 % and you get a message on an Android phone saying "GATT CMD STARTED", that might indicate a missing or incorrect bootloader. In this case do the following:
Go to New Project -> Gecko Bootloader -> Gecko Bootloader 1.5.0 and create that for your kit. Remember to choose the "Internal Storage Bootloader" option suitable for your storage size.
In the
.isc
-file for the bootloader project, you can configure some options, but for this example, pressGenerate
with the default settings.Build the project and find the folder in your bootloader project tree that is named
“GNU ARM <compiler version number> - Default”
. Flash thexxx-
combined.s37
-file to the device. This includes the first stage and main bootloaders.Now, proceed with flashing the
SOC - Empty
-project as in First steps #3.
Additional Resources
AN1086: Using the Gecko Bootloader with the Silicon Labs Bluetooth® Applications UG266: Silicon Labs Gecko Bootloader User's Guide