Adaptive Frequency Hopping
Introduction
Bluetooth works in the 2.4 GHz frequency range. Because this is an ISM band, it's highly likely to have interference with other devices working in the same frequency band. The Bluetooth standard makes it possible for the communicating devices to agree on which channels to use from the 37 available data channels during communication. If the master device detects high interference on a channel, it can initiate a channel map update. Adaptive frequency hopping (AFH) means that the communicating devices are continuously monitoring their environment for interference and are continuously changing the channel map to address the interference.
Note: AFH is a requirement for using TX power over +10 dBm. See Bluetooth Tx power settings.
Non-Adaptive Channel Blocking
Channel map update procedure is part of the Bluetooth 4.0 specification. This procedure makes it possible for the peer devices to agree on which channels they will use from the available 37 data channels during communication. Channel map update procedure can be initiated by the master only.
Being part of the Bluetooth 4.0 standard, this procedure is supported in all SDK versions. For example, if a smartphone connects to an EFR device, the smartphone, being a master, can disable some channels and the EFR will accept it. This feature is very often used to disable the Bluetooth channels that overlap with the Wi-Fi channel used by the smartphone.
However, when the EFR is the master, the EFR will enable all channels by default, without any restriction, and they can be disabled only manually. See section Manual Channel Blocking. Adaptive Frequency Hopping was introduced to overcome this issue and to block low-quality channels dynamically.
Interference Detection
Since Bluetooth SDK v2.9, adaptive frequency hopping can be enabled by calling gecko_init_afh();
after gecko_init(&config);
. (Note, that AFH implementation was in beta phase in Bluetooth SDK v2.9. Use Bluetooth SDK v2.10 or later for certifiable implementation.)
If AFH is enabled (and at least one advertiser is running with extended advertisements or at least one connection is active), the Bluetooth stack runs a periodic background task that sweeps all channels once every afh_scan_interval
and measures received power on each channel. If the measured power is beyond limit (-71 dBm) on a channel, the channel is blocked for at least 8 afh_scan_interval
s. (If interference is still found on the channel, the blocking is prolonged, i.e., unblocking of a channel needs 8 consecutive measurements with no interference detected.)
After each sweep, a new channel map is created based on the interference measurements. If the channel map has changed, the master device sends the new channel map to all slaves, using the channel map update process. Slaves cannot initiate channel map update.
ah_scan_interval
is set to 1 second by default and the sweep of the 40 channels takes around 10 ms, which means an additive energy consumption of ca. 240 uW.
Note: The AFH sweep has the highest priority among all Bluetooth operations. Therefore, if there are multiple operations within 10 ms, sweeping cannot be fitted between them and they may be blocked.
Additive energy consumption
Changing Scan Interval
afh_scan_interval
is set to 1 second by default, i.e., one channel sweep is made every second. Before Bluetooth SDK v2.11, this value was fixed. Since Bluetooth SDK v2.11, this value can be changed at any time by calling the following function:
#define AFH_SCAN_INTERVAL_CONFIG_KEY 7
uint8_t afh_scan_interval = 10; // set afh scan interval to 100ms
gecko_cmd_system_linklayer_configure(AFH_SCAN_INTERVAL_CONFIG_KEY,sizeof(uint8_t),&afh_scan_interval);
The unit of afh_scan_interval
is 10 ms.
Channel sweep is always done after a radio operation, e.g., after an advertisement is sent. Setting the scan interval e.g., to 100 ms does not mean that the sweep will be done every 100 ms but that after every radio operation the Bluetooth stack checks if at least 100 ms has passed since the last sweep. Let's say that afh_scan_interval
is set to 100 ms advertising is done with 80 ms advertisement interval. In this case, the scan is done after every second advertisement, i.e., once every 160 ms.
Manual Channel Blocking
Channels can also be blocked manually using the following command: gecko_cmd_le_gap_set_data_channel_classification()
. For details, see le_gap_set_data_channel_classification. If a channel is blocked manually, that channel will be never used until it is unblocked manually. In other words, the channels blocked by interference detection and channels blocked manually will be merged into a common channel map.
Transmit Power
You are allowed to use TX power above +10 dBm when AFH is enabled and at least 15 channels are available. See Bluetooth Tx power settings. However, note that high transmit power is only allowed once for each channel after a measurement on that channel occurs. In other words, if you use the same channel multiple times for transmitting within afh_scan_interval
, the second and consecutive transmission will use +10 dBm. If you have a short connection interval and long afh_scan_interval, this can easily happen. See the following figure:
screenshot of Energy profiler
Slave Adaptivity
To be ETSI compliant, slave devices need to be adaptive as well. The master might be non-adaptive, so the slave cannot blindly follow the transmissions of the master. ETSI allows using control transfer on blocked channels with +10 dBm or lower, but not data transfer. For ETSI compliance reasons, if the slave detects that a blocked channel is used, it will only send a single empty/control packet on that channel to prevent supervision timeout.
Frequency Hopping Algorithm
Bluetooth Low Energy has two channel selection algorithms. Algorithm #1 is the original and mandatory. Algorithm #2 was introduced with Bluetooth 5.0. The hopping algorithm used is chosen by the master at connection time. Algorithm #2 has more randomness so it is always used unless connecting to a legacy device.
- Algorithm #1: Channels are selected sequentially using fixed hop interval passed while establishing connection.
- Algorithm #2: The channel to be used is calculated from the current event counter and access address. The selected channel appears to be semi-random.
If a channel to be used is blocked on the channel map, the channel is remapped to an available channel using a remapping algorithm.
Other Limitations
When AFH is applied, the length of the connection events (not to be confused with the connection interval) is limited to 40 ms. In other words, in every connection interval you can send packets only for 40 ms. This is usually not a problem because it takes around 2.5 ms to transmit a packet with 251B payload. However, to achieve maximum throughput with unacknowledged data transmission (see Throughput with Bluetooth Low Energy, you have to take into account this limitation. For example, if you have 100 ms connection interval, you can send packets only 40% of the time. To achieve maximum throughput, decrease your connection interval to 40 ms or lower.