You are viewing documentation for version: 2.8 | 3.3 (latest) | Version History
User messaging (user)
This class provides one command and one event which can be utilized by a NCP host and target to implement a communication mechanism with own proprietary protocol. An application has the full responsibility on deciding whether
and how the command and event are used. The stack does not produce or consume any messages belonging to this class.
user commands
user_message_to_target
This command can be used by an NCP host to send a message to the target application on device.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0xff |
class |
Message class:User messaging |
3 |
0x00 |
method |
Message ID |
4 |
uint8array |
data |
The message |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0xff |
class |
Message class:User messaging |
3 |
0x00 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
6 |
uint8array |
data |
The response message |
API
/* Function */
struct gecko_msg_user_message_to_target_rsp_t *gecko_cmd_user_message_to_target(uint8 data_len, const uint8 *data_data);
/* Response id */
gecko_rsp_user_message_to_target_id
/* Response structure */
struct gecko_msg_user_message_to_target_rsp_t
{
uint16 result,
uint8array data
}
user events
user_message_to_host
This event can be used by the target application on device to send a message to NCP host.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0xff |
class |
Message class:User messaging |
3 |
0x00 |
method |
Message ID |
4 |
uint8array |
data |
The message |
API
/* event id*/
gecko_evt_user_message_to_host_id
/* event structure*/
struct gecko_msg_user_message_to_host_evt_t
{
uint8array data
}