Silicon Labs
bluetooth/2.9/error-codes
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
Results 1-5 of 5 for bluetooth/2.9/error-codes in 0.27 seconds
Error codes | Error Codes | Bluetooth LE | v2.13 | Silicon Labs
https://docs.silabs.com/....
You are viewing documentation for version: 2.13 Error codes# Errors related to hardware# ... error code indicates that an attempt to create a new ACL Connection to a
Status Codes | API Documentation | Platform | v5.0.2 | Silicon Labs
https://docs.silabs.com/.../sta...
You are viewing documentation for version: 5.0.2 Status Codes# Status Codes contains error and status code definitions used by Simplicity SDK ... Bluetooth cannot be used on this hardware.
Gecko Platform Release Notes
https://www.silabs.com/.../gecko-platform-release-notes-3.2.9.0....
Gecko Platform 3.2.9.0 GA Gecko SDK Suite 3.2 October 25, 2023 ... and public key validity checks will by default return an error code on EFR32xG21 parts with SE firmware before 1.2.2.
Resource TypeRelease Notes
Gecko Platform Release Notes 2.7.10.0
https://www.silabs.com/.../gecko-platform-release-notes-2.7.10.0....
... defines for more SE error codes to em_se.h. Added in release 2.7.2.0 A version check has been added to ... for Bluetooth LE AoX. Added in release 2.7.3.0 Revamped Features and rail_features.h ...
Resource TypeRelease Notes
Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
https://docs.silabs.com/.../sl-bt-adverti...
Training ... Register // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... Wrong state error is returned if advertising has been enabled on the advertising set.
    Results 1-5 of 5 for bluetooth/2.9/error-codes