You are viewing documentation for version: 2.9 | Version History
Connection management (le_connection)
The commands and events in this class are related to managing connection establishment, parameter setting, and disconnection procedures.
le_connection commands
le_connection_close
This command can be used to close a Bluetooth connection or cancel an ongoing connection establishment process. The parameter is a connection handle which is reported in
le_connection_opened event or le_gap_open response.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x04 |
method |
Message ID |
4 |
uint8 |
connection |
Handle of the connection to be closed |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x04 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_le_connection_close_rsp_t *gecko_cmd_le_connection_close(uint8 connection);
/* Response id */
gecko_rsp_le_connection_close_id
/* Response structure */
struct gecko_msg_le_connection_close_rsp_t
{
uint16 result
}
Events generated
le_connection_disable_slave_latency
This command temporarily enables or disables slave latency. Used only when Bluetooth device is in slave role.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x02 |
method |
Message ID |
4 |
uint8 |
connection |
Connection Handle |
5 |
uint8 |
disable |
0 enable, 1 disable slave latency |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x02 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_le_connection_disable_slave_latency_rsp_t *gecko_cmd_le_connection_disable_slave_latency(uint8 connection, uint8 disable);
/* Response id */
gecko_rsp_le_connection_disable_slave_latency_id
/* Response structure */
struct gecko_msg_le_connection_disable_slave_latency_rsp_t
{
uint16 result
}
le_connection_get_rssi
This command can be used to get the latest RSSI value of a Bluetooth connection.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x01 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x01 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x01 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_le_connection_get_rssi_rsp_t *gecko_cmd_le_connection_get_rssi(uint8 connection);
/* Response id */
gecko_rsp_le_connection_get_rssi_id
/* Response structure */
struct gecko_msg_le_connection_get_rssi_rsp_t
{
uint16 result
}
Events generated
le_connection_set_parameters
This command can be used to request a change in the connection parameters of a Bluetooth connection.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x09 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x00 |
method |
Message ID |
4 |
uint8 |
connection |
Connection Handle |
5-6 |
uint16 |
min_interval |
Minimum value for the connection event interval. This must be set be less than or equal to max_interval.
- Time = Value x 1.25 ms
- Range: 0x0006 to 0x0c80
- Time Range: 7.5 ms to 4 s
|
7-8 |
uint16 |
max_interval |
Maximum value for the connection event interval. This must be set greater than or equal to min_interval.
- Time = Value x 1.25 ms
- Range: 0x0006 to 0x0c80
- Time Range: 7.5 ms to 4 s
|
9-10 |
uint16 |
latency |
Slave latency. This parameter defines how many connection intervals the slave can skip if it has no data to send
Use 0x0000 for default value
|
11-12 |
uint16 |
timeout |
Supervision timeout. The supervision timeout defines for how long the connection is maintained despite the devices being unable to communicate at the currently configured connection intervals.
- Range: 0x000a to 0x0c80
- Time = Value x 10 ms
- Time Range: 100 ms to 32 s
- The value in milliseconds must be larger than (1 + latency) * max_interval * 2, where max_interval is given in milliseconds
It is recommended that the supervision timeout is set at a value which allows communication attempts over at least a few connection intervals.
|
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x00 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_le_connection_set_parameters_rsp_t *gecko_cmd_le_connection_set_parameters(uint8 connection, uint16 min_interval, uint16 max_interval, uint16 latency, uint16 timeout);
/* Response id */
gecko_rsp_le_connection_set_parameters_id
/* Response structure */
struct gecko_msg_le_connection_set_parameters_rsp_t
{
uint16 result
}
Events generated
Event |
Description |
le_connection_parameters
|
This event is triggered after new connection parameters has been applied on the connection. |
le_connection_set_phy
This command can be used to set preferred PHYs for connection. Preferred PHYs are connection specific. Event
le_connection_phy_status is received when PHY update procedure has been completed. Other than preferred PHY can also be set if remote device does not accept any of the preferred PHYs.
NOTE: 2 Mbit and Coded PHYs are not supported by all devices.
Command
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Command |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x03 |
method |
Message ID |
4 |
uint8 |
connection |
|
5 |
uint8 |
phy |
Preferred PHYs for connection. This parameter is bitfield and multiple PHYs can be preferred by setting multiple bits.
-
0x01: 1 Mbit PHY
-
0x02: 2 Mbit PHY
-
0x04: 125 kbit Coded PHY (S=8)
-
0x08: 500 kbit Coded PHY (S=2)
|
Response
Byte |
Type |
Name |
Description |
0 |
0x20 |
hilen |
Message type: Response |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x03 |
method |
Message ID |
4-5 |
uint16 |
result |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
API
/* Function */
struct gecko_msg_le_connection_set_phy_rsp_t *gecko_cmd_le_connection_set_phy(uint8 connection, uint8 phy);
/* Response id */
gecko_rsp_le_connection_set_phy_id
/* Response structure */
struct gecko_msg_le_connection_set_phy_rsp_t
{
uint16 result
}
Events generated
le_connection events
le_connection_opened
This event indicates that a new connection was opened, whether the devices are already bonded, and what is the role of the Bluetooth device (Slave or Master). An open connection can be closed with the
le_connection_close command by giving the connection handle ID obtained from this event.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x0b |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x00 |
method |
Message ID |
4-9 |
bd_addr |
address |
Remote device address |
10 |
uint8 |
address_type
|
Remote device address type |
11 |
uint8 |
master |
Device role in connection. Values:
|
12 |
uint8 |
connection |
Handle for new connection |
13 |
uint8 |
bonding |
Bonding handle. Values:
-
0xff: No bonding
-
Other: Bonding handle
|
14 |
uint8 |
advertiser |
The local advertising set this connection was opened to. Values:
-
0xff: Invalid value or not applicable, and this field should be ignored
-
Other: The advertising set handle
|
API
/* event id*/
gecko_evt_le_connection_opened_id
/* event structure*/
struct gecko_msg_le_connection_opened_evt_t
{
bd_addr address,
uint8 address_type,
uint8 master,
uint8 connection,
uint8 bonding,
uint8 advertiser
}
le_connection_closed
This event indicates that a connection was closed.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x03 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x01 |
method |
Message ID |
4-5 |
uint16 |
reason |
Result code
-
0: success
-
Non-zero: an error occurred
For other values refer to the
Error codes
|
6 |
uint8 |
connection |
Handle of the closed connection |
API
/* event id*/
gecko_evt_le_connection_closed_id
/* event structure*/
struct gecko_msg_le_connection_closed_evt_t
{
uint16 reason,
uint8 connection
}
le_connection_parameters
This event is triggered whenever the connection parameters are changed and at any time a connection is established.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x0a |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x02 |
method |
Message ID |
4 |
uint8 |
connection |
Connection handle |
5-6 |
uint16 |
interval |
Connection interval |
7-8 |
uint16 |
latency |
Slave latency |
9-10 |
uint16 |
timeout |
Supervision timeout |
11 |
uint8 |
security_mode
|
Connection security mode |
12-13 |
uint16 |
txsize |
Maximum Data Channel PDU Payload size the controller can send in an air packet |
API
/* event id*/
gecko_evt_le_connection_parameters_id
/* event structure*/
struct gecko_msg_le_connection_parameters_evt_t
{
uint8 connection,
uint16 interval,
uint16 latency,
uint16 timeout,
uint8 security_mode,
uint16 txsize
}
le_connection_phy_status
This event indicates that PHY update procedure has been completed.
Event
Byte |
Type |
Name |
Description |
0 |
0xa0 |
hilen |
Message type: Event |
1 |
0x02 |
lolen |
Minimum payload length |
2 |
0x08 |
class |
Message class:Connection management |
3 |
0x04 |
method |
Message ID |
4 |
uint8 |
connection |
|
5 |
uint8 |
phy |
Current active PHY. See values from
le_connection_set_phy command. |
API
/* event id*/
gecko_evt_le_connection_phy_status_id
/* event structure*/
struct gecko_msg_le_connection_phy_status_evt_t
{
uint8 connection,
uint8 phy
}
le_connection enumerations
le_connection_security
These values indicate the Bluetooth Security Mode.
Enumerations
Value |
Name |
Description |
0 |
le_connection_mode1_level1 |
No security |
1 |
le_connection_mode1_level2 |
Unauthenticated pairing with encryption |
2 |
le_connection_mode1_level3 |
Authenticated pairing with encryption |
3 |
le_connection_mode1_level4 |
Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key |