System (system)
The commands and events in this class can be used to access and query the local device.system commands
system_get_bt_address
This command can be used to read the Bluetooth public address used by the device.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x00 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x03 | method | Message ID |
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x06 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x03 | method | Message ID |
4-9 | bd_addr | address | Bluetooth public address in little endian format |
API
/* Function */
struct gecko_msg_system_get_bt_address_rsp_t *gecko_cmd_system_get_bt_address();
/* Response id */
gecko_rsp_system_get_bt_address_id
/* Response structure */
struct gecko_msg_system_get_bt_address_rsp_t
{
bd_addr address
}
system_get_counters
Get packet and error counters
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x01 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0f | method | Message ID |
4 | uint8 | reset | Reset counters if parameter value is nonzero |
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x0a | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0f | method | Message ID |
4-5 | uint16 | result |
Result code
|
6-7 | uint16 | tx_packets | Number of successfully transmitted packets |
8-9 | uint16 | rx_packets | Number of successfully received packets |
10-11 | uint16 | crc_errors | Number of received packets with CRC errors |
12-13 | uint16 | failures | Number of radio failures like aborted tx/rx packets, scheduling failures, etc |
API
/* Function */
struct gecko_msg_system_get_counters_rsp_t *gecko_cmd_system_get_counters(uint8 reset);
/* Response id */
gecko_rsp_system_get_counters_id
/* Response structure */
struct gecko_msg_system_get_counters_rsp_t
{
uint16 result,
uint16 tx_packets,
uint16 rx_packets,
uint16 crc_errors,
uint16 failures
}
system_get_random_data
This command can be used to get random data up to 16 bytes.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x01 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0b | method | Message ID |
4 | uint8 | length | Length of random data. Maximum length is 16 bytes. |
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x03 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0b | method | Message ID |
4-5 | uint16 | result |
Result code
|
6 | uint8array | data | Random data |
API
/* Function */
struct gecko_msg_system_get_random_data_rsp_t *gecko_cmd_system_get_random_data(uint8 length);
/* Response id */
gecko_rsp_system_get_random_data_id
/* Response structure */
struct gecko_msg_system_get_random_data_rsp_t
{
uint16 result,
uint8array data
}
system_halt
This command forces radio to idle state and allows device to sleep. Advertising, scanning, connections and software timers are halted by this commands. Halted operations are resumed by calling this command with parameter 0. Connections stay alive if system is resumed before connection supervision timeout.
NOTE:Software timer is also halted. Hardware interrupts are the only way to wake up from energy mode 2 when system is halted.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x01 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0c | method | Message ID |
4 | uint8 | halt |
Values:
|
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0c | method | Message ID |
4-5 | uint16 | result |
Result code
|
API
/* Function */
struct gecko_msg_system_halt_rsp_t *gecko_cmd_system_halt(uint8 halt);
/* Response id */
gecko_rsp_system_halt_id
/* Response structure */
struct gecko_msg_system_halt_rsp_t
{
uint16 result
}
system_hello
This command does not trigger any event but the response to the command is used to verify that communication between the host and the device is working.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x00 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x00 | method | Message ID |
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x00 | method | Message ID |
4-5 | uint16 | result |
Result code
|
API
/* Function */
struct gecko_msg_system_hello_rsp_t *gecko_cmd_system_hello();
/* Response id */
gecko_rsp_system_hello_id
/* Response structure */
struct gecko_msg_system_hello_rsp_t
{
uint16 result
}
system_reset
This command can be used to reset the system. It does not have a response, but it triggers one of the boot events (normal reset or boot to DFU mode) depending on the selected boot mode.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x01 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x01 | method | Message ID |
4 | uint8 | dfu | Boot mode:
|
Command does not have response
API
/* Function */
void *gecko_cmd_system_reset(uint8 dfu);
/* Command does not have response */
Events generated
Event | Description |
---|---|
system_boot | Sent after the device has booted into normal mode |
dfu_boot | Sent after the device has booted into UART DFU mode |
system_set_bt_address
This command can be used to set the Bluetooth public address used by the device. A valid address set with this command overrides the default Bluetooth public address programmed at production, and it will be effective in the next system reboot. The stack treats 00:00:00:00:00:00 and ff:ff:ff:ff:ff:ff as invalid addresses. Thus passing one of them into this command will cause the stack to use the default address in the next system reboot.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x06 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x04 | method | Message ID |
4-9 | bd_addr | address | Bluetooth public address in little endian format |
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x04 | method | Message ID |
4-5 | uint16 | result |
Result code
|
API
/* Function */
struct gecko_msg_system_set_bt_address_rsp_t *gecko_cmd_system_set_bt_address(bd_addr address);
/* Response id */
gecko_rsp_system_set_bt_address_id
/* Response structure */
struct gecko_msg_system_set_bt_address_rsp_t
{
uint16 result
}
system_set_device_name
This command can be used to set the device name. Currently it is possible to set the name which will be used during the OTA update. The name will be stored in persistent storage. If the OTA device name is also set in gecko configuration, the name stored in persistent storage is overwritten with the name in gecko configuration during device boot.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0d | method | Message ID |
4 | uint8 | type | Device name to set. Values:
|
5 | uint8array | name | Device name |
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0d | method | Message ID |
4-5 | uint16 | result |
Result code
|
API
/* Function */
struct gecko_msg_system_set_device_name_rsp_t *gecko_cmd_system_set_device_name(uint8 type, uint8 name_len, const uint8 *name_data);
/* Response id */
gecko_rsp_system_set_device_name_id
/* Response structure */
struct gecko_msg_system_set_device_name_rsp_t
{
uint16 result
}
system_set_tx_power
This command can be used to set the global maximum TX power for Bluetooth. The returned value in the response is the selected maximum output power level after applying RF path compensation. If the GATT server contains a Tx Power service, the Tx Power Level attribute of the service will be updated accordingly.
The selected power level may be less than the specified value if the device does not meet the power requirements. For Bluetooth connections the maximum TX power will be limited to 10 dBm if Adaptive Frequency Hopping (AFH) is not enabled.
By default, the global maximum TX power value is 8 dBm.
NOTE: This command should not be used while advertising, scanning or during connection.
Command
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Command |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0a | method | Message ID |
4-5 | int16 | power | TX power in 0.1dBm steps, for example the value of 10 is 1dBm and 55 is 5.5dBm |
Response
Byte | Type | Name | Description |
---|---|---|---|
0 | 0x20 | hilen | Message type: Response |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x0a | method | Message ID |
4-5 | int16 | set_power | The selected maximum power level |
API
/* Function */
struct gecko_msg_system_set_tx_power_rsp_t *gecko_cmd_system_set_tx_power(int16 power);
/* Response id */
gecko_rsp_system_set_tx_power_id
/* Response structure */
struct gecko_msg_system_set_tx_power_rsp_t
{
int16 set_power
}
system events
system_boot
This event indicates the device has started and the radio is ready. This even carries the firmware build number and other SW and HW identification codes.
Event
Byte | Type | Name | Description |
---|---|---|---|
0 | 0xa0 | hilen | Message type: Event |
1 | 0x12 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x00 | method | Message ID |
4-5 | uint16 | major | Major release version |
6-7 | uint16 | minor | Minor release version |
8-9 | uint16 | patch | Patch release number |
10-11 | uint16 | build | Build number |
12-15 | uint32 | bootloader | Bootloader version |
16-17 | uint16 | hw | Hardware type |
18-21 | uint32 | hash | Version hash |
API
/* event id*/
gecko_evt_system_boot_id
/* event structure*/
struct gecko_msg_system_boot_evt_t
{
uint16 major,
uint16 minor,
uint16 patch,
uint16 build,
uint32 bootloader,
uint16 hw,
uint32 hash
}
system_external_signal
This event indicates external signals have been received. External signals are generated from native application.
Event
Byte | Type | Name | Description |
---|---|---|---|
0 | 0xa0 | hilen | Message type: Event |
1 | 0x04 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x03 | method | Message ID |
4-7 | uint32 | extsignals | Bitmask of external signals received since last event. |
API
/* event id*/
gecko_evt_system_external_signal_id
/* event structure*/
struct gecko_msg_system_external_signal_evt_t
{
uint32 extsignals
}
system_awake
This event indicates that the device has woken up from sleep mode.
NOTE: Stack does not generate this event by itself as sleep and wakeup are managed in applications. If this event is needed, the application should call function gecko_send_system_awake() to signal stack to send this event.
Event
Byte | Type | Name | Description |
---|---|---|---|
0 | 0xa0 | hilen | Message type: Event |
1 | 0x00 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x04 | method | Message ID |
API
/* event id*/
gecko_evt_system_awake_id
/* event structure*/
struct gecko_msg_system_awake_evt_t
{
}
system_hardware_error
This event indicates that hardware related errors occurred.
Event
Byte | Type | Name | Description |
---|---|---|---|
0 | 0xa0 | hilen | Message type: Event |
1 | 0x02 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x05 | method | Message ID |
4-5 | uint16 | status |
Result code
|
API
/* event id*/
gecko_evt_system_hardware_error_id
/* event structure*/
struct gecko_msg_system_hardware_error_evt_t
{
uint16 status
}
system_error
This event indicates errors.
Event
Byte | Type | Name | Description |
---|---|---|---|
0 | 0xa0 | hilen | Message type: Event |
1 | 0x03 | lolen | Minimum payload length |
2 | 0x01 | class | Message class:System |
3 | 0x06 | method | Message ID |
4-5 | uint16 | reason | Standard code of the error just happened. |
6 | uint8array | data | Data related to the error, this field can be empty. |
API
/* event id*/
gecko_evt_system_error_id
/* event structure*/
struct gecko_msg_system_error_evt_t
{
uint16 reason,
uint8array data
}