Coexistence#
Coexistence.
Enumerations | |
|---|---|
Coexistence Options. | |
enum | coex_option_t { coex_option_enable = 0x100, coex_option_tx_abort = 0x400, coex_option_high_priority = 0x800 } |
Functions | |
|---|---|
sl_status_t | sl_bt_coex_set_options (uint32_t mask, uint32_t options) |
sl_status_t | sl_bt_coex_set_parameters (uint8_t priority, uint8_t request, uint8_t pwm_period, uint8_t pwm_dutycycle) |
sl_status_t | sl_bt_coex_set_directional_priority_pulse (uint8_t pulse) |
sl_status_t | sl_bt_coex_get_counters (uint8_t reset, size_t max_counters_size, size_t *counters_len, uint8_t *counters) |
Detailed Description#
Coexistence.
Coexistence BGAPI class. Coexistence interface is enabled and initialized with sl_bt_init_coex_hal function.
Enumeration Type Documentation#
coex_option_t#
enum coex_option_t
Coexistence Options.
Enumerator | |
|---|---|
coex_option_enable | (0x100) Enable coexistence feature |
coex_option_tx_abort | (0x400) Abort transmission if grant is denied |
coex_option_high_priority | (0x800) Enable priority signal |
Function Documentation#
sl_bt_coex_set_options()#
sl_status_t sl_bt_coex_set_options | ( | uint32_t |
|
uint32_t |
| ||
) |
Configure coexistence options at runtime.
Parameters
[in] |
| Enum coex_option_t. Mask defines which coexistence options are changed. |
[in] |
| Enum coex_option_t. Value of options to be changed. This parameter is used together with the mask parameter. |
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_coex_set_parameters()#
sl_status_t sl_bt_coex_set_parameters | ( | uint8_t |
|
uint8_t |
| ||
uint8_t |
| ||
uint8_t |
| ||
) |
Configure coexistence parameters.
Parameters
[in] |
| Coexistence priority threshold. Coexistence priority is toggled if priority is below this value. |
[in] |
| Coexistence request threshold. Coexistence request is toggled if priority is below this value. |
[in] |
| PWM functionality period length in 1ms units |
[in] |
| PWM functionality dutycycle in percentage |
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_coex_set_directional_priority_pulse()#
sl_status_t sl_bt_coex_set_directional_priority_pulse ( uint8_t
pulse)
Set Directional Priority Pulse Width
Parameters
[in] |
| Directional priority pulse width in us |
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_coex_get_counters()#
sl_status_t sl_bt_coex_get_counters | ( | uint8_t |
|
size_t |
| ||
size_t * |
| ||
uint8_t * |
| ||
) |
Read coexistence statistic counters from the device. Response contains the list of uint32 type counter values. Counters in the list are in following order: low priority requested, high priority requested, low priority denied, high priority denied, low-priority TX aborted, and high-priority TX aborted. Passing a non-zero value also resets counters.
Parameters
[in] |
| Reset counters if parameter value is not zero. |
[in] |
| Size of output buffer passed in |
[out] |
| On return, set to the length of output data written to |
[out] |
| Coexistence statistic counters |
Returns
SL_STATUS_OK if successful. Error code otherwise.