Advertiser.
Modules | |
| sl_bt_evt_advertiser_timeout | |
| Indicates that the advertiser has completed the configured number of advertising events in the advertising set and advertising has stopped. | |
| sl_bt_evt_advertiser_scan_request | |
| Reports any scan request received in advertising mode if the scan request notification is enabled. | |
Enumerations | |
| enum | advertiser_connectable_mode_t { advertiser_non_connectable = 0x0, advertiser_directed_connectable = 0x1, advertiser_connectable_scannable = 0x2, advertiser_scannable_non_connectable = 0x3, advertiser_connectable_non_scannable = 0x4 } |
| Advertiser Connectable Mode. | |
| enum | advertiser_discoverable_mode_t { advertiser_non_discoverable = 0x0, advertiser_limited_discoverable = 0x1, advertiser_general_discoverable = 0x2, advertiser_broadcast = 0x3, advertiser_user_data = 0x4 } |
| Advertiser Discoverable Mode. | |
| enum | advertiser_adv_address_type_t { advertiser_identity_address = 0x0, advertiser_non_resolvable = 0x1 } |
| Advertising Address Type. | |
Functions | |
| sl_status_t | sl_bt_advertiser_create_set (uint8_t *handle) |
| sl_status_t | sl_bt_advertiser_set_timing (uint8_t handle, uint32_t interval_min, uint32_t interval_max, uint16_t duration, uint8_t maxevents) |
| sl_status_t | sl_bt_advertiser_set_phy (uint8_t handle, uint8_t primary_phy, uint8_t secondary_phy) |
| sl_status_t | sl_bt_advertiser_set_channel_map (uint8_t handle, uint8_t channel_map) |
| sl_status_t | sl_bt_advertiser_set_tx_power (uint8_t handle, int16_t power, int16_t *set_power) |
| sl_status_t | sl_bt_advertiser_set_report_scan_request (uint8_t handle, uint8_t report_scan_req) |
| sl_status_t | sl_bt_advertiser_set_random_address (uint8_t handle, uint8_t addr_type, bd_addr address, bd_addr *address_out) |
| sl_status_t | sl_bt_advertiser_clear_random_address (uint8_t handle) |
| sl_status_t | sl_bt_advertiser_set_configuration (uint8_t handle, uint32_t configurations) |
| sl_status_t | sl_bt_advertiser_clear_configuration (uint8_t handle, uint32_t configurations) |
| sl_status_t | sl_bt_advertiser_set_data (uint8_t handle, uint8_t packet_type, size_t adv_data_len, const uint8_t *adv_data) |
| sl_status_t | sl_bt_advertiser_set_long_data (uint8_t handle, uint8_t packet_type) |
| sl_status_t | sl_bt_advertiser_start (uint8_t handle, uint8_t discover, uint8_t connect) |
| sl_status_t | sl_bt_advertiser_stop (uint8_t handle) |
| sl_status_t | sl_bt_advertiser_start_periodic_advertising (uint8_t handle, uint16_t interval_min, uint16_t interval_max, uint32_t flags) |
| sl_status_t | sl_bt_advertiser_stop_periodic_advertising (uint8_t handle) |
| sl_status_t | sl_bt_advertiser_delete_set (uint8_t handle) |
Advertiser.
The commands and events in this class are related to advertising functionalities in GAP peripheral and broadcaster roles.
Advertiser Connectable Mode.
Advertiser Discoverable Mode.
| sl_status_t sl_bt_advertiser_create_set | ( | uint8_t * | handle | ) |
Create an advertising set. The handle of the created advertising set is returned in response.
| [out] | handle | Advertising set handle |
| sl_status_t sl_bt_advertiser_set_timing | ( | uint8_t | handle, |
| uint32_t | interval_min, |
||
| uint32_t | interval_max, |
||
| uint16_t | duration, |
||
| uint8_t | maxevents |
||
| ) |
Set the advertising timing parameters of the given advertising set. This setting will take effect next time that advertising is enabled.
| [in] | handle | Advertising set handle |
| [in] | interval_min | Minimum advertising interval. Value in units of 0.625 ms
Default value: 100 ms |
| [in] | interval_max | Maximum advertising interval. Value in units of 0.625 ms
Default value: 200 ms |
| [in] | duration | Advertising duration for this advertising set. Value 0 indicates no advertising duration limit and advertising continues until it is disabled. A non-zero value sets the duration in units of 10 ms. The duration begins at the start of the first advertising event of this advertising set.
Default value: 0 |
| [in] | maxevents | If non-zero, indicates the maximum number of advertising events to send before the advertiser is stopped. Value 0 indicates no maximum number limit. Default value: 0 |
| sl_status_t sl_bt_advertiser_set_phy | ( | uint8_t | handle, |
| uint8_t | primary_phy, |
||
| uint8_t | secondary_phy |
||
| ) |
Set advertising PHYs of the given advertising set. This setting will take effect next time that advertising is enabled. The invalid parameter error is returned if a PHY value is invalid or the device does not support a given PHY.
| [in] | handle | Advertising set handle |
| [in] | primary_phy | Enum gap_phy_type_t. The PHY on which the advertising packets are transmitted on the primary advertising channel. If legacy advertising PDUs are used, 1M PHY must be used. Values:
Default value: gap_1m_phy |
| [in] | secondary_phy | Enum gap_phy_type_t. The PHY on which the advertising packets are transmitted on the secondary advertising channel. Values:
Default value: gap_1m_phy |
| sl_status_t sl_bt_advertiser_set_channel_map | ( | uint8_t | handle, |
| uint8_t | channel_map |
||
| ) |
Set the primary advertising channel map of the given advertising set. This setting will take effect next time that advertising is enabled.
| [in] | handle | Advertising set handle |
| [in] | channel_map | Advertising channel map which determines which of the three channels will be used for advertising. This value is given as a bitmask. Values:
Recommended value: 7 Default value: 7 |
| sl_status_t sl_bt_advertiser_set_tx_power | ( | uint8_t | handle, |
| int16_t | power, |
||
| int16_t * | set_power |
||
| ) |
Limit the maximum advertising TX power on the given advertising set. If the value goes over the global value that was set using sl_bt_system_set_max_tx_power command, the global value will be the maximum limit. The maximum TX power of legacy advertising is further constrained to be less than +10 dBm. Extended advertising TX power can be +10 dBm and over if Adaptive Frequency Hopping is enabled.
This setting will take effect next time advertising is enabled.
By default, maximum advertising TX power is limited by the global value.
| [in] | handle | Advertising set handle |
| [in] | power | TX power in 0.1 dBm steps. For example, the value of 10 is 1 dBm and 55 is 5.5 dBm. |
| [out] | set_power | The selected maximum advertising TX power |
| sl_status_t sl_bt_advertiser_set_report_scan_request | ( | uint8_t | handle, |
| uint8_t | report_scan_req |
||
| ) |
Enable or disable the scan request notification of a given advertising set. This setting will take effect next time that advertising is enabled.
| [in] | handle | Advertising set handle |
| [in] | report_scan_req | If non-zero, enables scan request notification and scan requests will be reported as events. Default value: 0 |
Events
| sl_status_t sl_bt_advertiser_set_random_address | ( | uint8_t | handle, |
| uint8_t | addr_type, |
||
| bd_addr | address, |
||
| bd_addr * | address_out |
||
| ) |
Set the advertiser on an advertising set to use a random address. This overrides the default advertiser address which is either the public device address programmed at production or the address written into persistent storage using sl_bt_system_set_identity_address command. This setting is stored in RAM only and does not change the identity address in persistent storage.
When setting a resolvable random address, the address parameter is ignored. The stack generates a private resolvable random address and set it as the advertiser address. The generated address is returned in the response.
To use the default advertiser address, remove this setting using sl_bt_advertiser_clear_random_address command.
Wrong state error is returned if advertising has been enabled on the advertising set. Invalid parameter error is returned if the advertising set handle is invalid or the address does not conforms to the Bluetooth specification.
| [in] | handle | Advertising set handle |
| [in] | addr_type | Address type:
|
| [in] | address | The random address to set. Ignore this field when setting a resolvable random address. |
| [out] | address_out | The resolvable random address set for the advetiser. Ignore this field when setting other types of random address. |
| sl_status_t sl_bt_advertiser_clear_random_address | ( | uint8_t | handle | ) |
Clear the random address previously set for the advertiser address on an advertising set. A random address can be set using sl_bt_advertiser_set_random_address command. The default advertiser address will be used after this operation.
Wrong state error is returned if advertising has been enabled on the advertising set. Invalid parameter error is returned if the advertising set handle is invalid.
| [in] | handle | Advertising set handle |
| sl_status_t sl_bt_advertiser_set_configuration | ( | uint8_t | handle, |
| uint32_t | configurations |
||
| ) |
Enable advertising configuration flags on the given advertising set. The configuration change will take effect next time that advertising is enabled.
These configuration flags can be disabled using sl_bt_advertiser_clear_configuration.
| [in] | handle | Advertising set handle |
| [in] | configurations | Advertising configuration flags to enable. This value can be a bitmask of multiple flags. Flags:
Default value: 1 |
| sl_status_t sl_bt_advertiser_clear_configuration | ( | uint8_t | handle, |
| uint32_t | configurations |
||
| ) |
Disable advertising configuration flags on the given advertising set. The configuration change will take effect next time that advertising is enabled.
These configuration flags can be enabled using sl_bt_advertiser_set_configuration.
| [in] | handle | Advertising set handle |
| [in] | configurations | Advertising configuration flags to disable. This value can be a bitmask of multiple flags. See sl_bt_advertiser_set_configuration for possible flags. |
| sl_status_t sl_bt_advertiser_set_data | ( | uint8_t | handle, |
| uint8_t | packet_type, |
||
| size_t | adv_data_len, |
||
| const uint8_t * | adv_data |
||
| ) |
Set user-defined data in advertising packets, scan response packets, or periodic advertising packets. Maximum 31 bytes of data can be set for legacy advertising. Maximum 191 bytes of data can be set for connectable extended advertising. Maximum 253 bytes of data can be set for periodic and non-connectable extended advertising. For setting longer advertising data, use command sl_bt_advertiser_set_long_data.
If advertising mode is currently enabled, the new advertising data will be used immediately. Advertising mode can be enabled using command sl_bt_advertiser_start. Periodic advertising mode can be enabled using command sl_bt_advertiser_start_periodic_advertising.
The invalid parameter error will be returned in the following situations:
Note that the user-defined data may be overwritten by the system when the advertising is later enabled in a discoverable mode other than user_data.
| [in] | handle | Advertising set handle |
| [in] | packet_type | This value selects whether data is intended for advertising packets, scan response packets or periodic advertising packets.
|
| [in] | adv_data_len | Array length |
| [in] | adv_data | Data to be set |
| sl_status_t sl_bt_advertiser_set_long_data | ( | uint8_t | handle, |
| uint8_t | packet_type |
||
| ) |
Set advertising data for a specified packet type and advertising set. Data currently in the system data buffer will be extracted as the advertising data. The buffer will be emptied after this command regardless of the completion status.
Prior to calling this command, add data to the buffer with one or multiple calls of sl_bt_system_data_buffer_write.
Maximum 31 bytes of data can be set for legacy advertising. Maximum 191 bytes of data can be set for connectable extended advertising. Maximum 1650 bytes of data can be set for periodic and non-connectable extended advertising, but advertising parameters may limit the amount of data that can be sent in a single advertisement.
See sl_bt_advertiser_set_data for more details on advertising data.
| [in] | handle | Advertising set handle |
| [in] | packet_type | This value selects whether data is intended for advertising packets, scan response packets, or periodic advertising packets. Values:
|
| sl_status_t sl_bt_advertiser_start | ( | uint8_t | handle, |
| uint8_t | discover, |
||
| uint8_t | connect |
||
| ) |
Start advertising of a given advertising set with specified discoverable and connectable modes.
The number of concurrent advertising is limited by MAX_ADVERTISERS configuration.
The number of concurrent connectable advertising is also limited by MAX_CONNECTIONS configuration. For example, only one connectable advertising can be enabled if the device has (MAX_CONNECTIONS - 1) connections when this command is called. The limitation does not apply to non-connectable advertising.
The default advertising configuration in the stack is set to using legacy advertising PDUs on 1M PHY. The stack will automatically select extended advertising PDUs if either of the following has occurred with the default configuration:
If currently set parameters can't be used, an error is returned. Specifically, this command fails with the connection limit exceeded error if it causes the number of connections exceeding the configured MAX_CONNECTIONS value. It fails with the invalid parameter error if one of the following use cases occurs:
If advertising is enabled in user_data mode, use sl_bt_advertiser_set_data to set advertising and scan response data before issuing this command. When advertising is enabled in modes other than user_data, advertising and scan response data is generated by the stack using the following procedure:
Event sl_bt_evt_connection_opened will be received when a remote device opens a connection to the advertiser on this advertising set and also advertising on the given set stops.
Event sl_bt_evt_advertiser_timeout will be received when the number of advertising events set by sl_bt_advertiser_set_timing command is done and advertising with the current set has stopped.
| [in] | handle | Advertising set handle |
| [in] | discover | Enum advertiser_discoverable_mode_t. Discoverable mode. Values:
|
| [in] | connect | Enum advertiser_connectable_mode_t. Connectable mode. Values:
|
Events
| sl_status_t sl_bt_advertiser_stop | ( | uint8_t | handle | ) |
Stop the advertising of the given advertising set. Counterpart with sl_bt_advertiser_start.
This command does not affect the enable state of the periodic advertising set, i.e., periodic advertising is not stopped.
| [in] | handle | Advertising set handle |
| sl_status_t sl_bt_advertiser_start_periodic_advertising | ( | uint8_t | handle, |
| uint16_t | interval_min, |
||
| uint16_t | interval_max, |
||
| uint32_t | flags |
||
| ) |
Start periodic advertising on the given advertising set. The stack enables the advertising set automatically if the set was not enabled and the set can advertise using extended advertising PDUs beside the syncInfo (which is needed for the periodic advertising).
The invalid parameter error is returned if the application has configured legacy advertising PDUs or anonymous advertising, or the advertising set is enabled using legacy advertising PDUs.
To stop periodic advertising, use sl_bt_advertiser_stop_periodic_advertising command with the handle received in response from this command.
| [in] | handle | Advertising set handle |
| [in] | interval_min | Minimum periodic advertising interval. Value in units of 1.25 ms
Default value: 100 ms |
| [in] | interval_max | Maximum periodic advertising interval. Value in units of 1.25 ms
Default value: 200 ms |
| [in] | flags | Periodic advertising configurations. Bitmask of the following:
|
| sl_status_t sl_bt_advertiser_stop_periodic_advertising | ( | uint8_t | handle | ) |
Stop the periodic advertising on the given advertising set. Counterpart with sl_bt_advertiser_start_periodic_advertising.
This command does not affect the enable state of the advertising set, i.e., legacy or extended advertising is not stopped.
| [in] | handle | Advertising set handle |
| sl_status_t sl_bt_advertiser_delete_set | ( | uint8_t | handle | ) |
Delete an advertising set.
| [in] | handle | Advertising set handle |