Coexistence.
Coexistence.
Coexistence BGAPI class. Coexistence interface is enabled and initialized with sl_bt_init_coex_hal function.
◆ coex_option_t
Coexistence Options.
| Enumerator |
|---|
| coex_option_enable | (0x100) Enable coexistence feature
|
| coex_option_tx_abort | (0x400) Abort transmission if grant is denied
|
| coex_option_high_priority | (0x800) Enable priority signal
|
◆ sl_bt_coex_set_options()
| sl_status_t sl_bt_coex_set_options |
( |
uint32_t |
mask, |
|
|
uint32_t |
options |
|
) |
| |
Configure coexistence options at runtime.
- Parameters
-
| [in] | mask | Enum coex_option_t. Mask defines which coexistence options are changed. |
| [in] | options | Enum coex_option_t. Value of options to be changed. This parameter is used together with the mask parameter. |
- Returns
- SL_STATUS_OK if successful. Error code otherwise.
◆ sl_bt_coex_set_parameters()
| sl_status_t sl_bt_coex_set_parameters |
( |
uint8_t |
priority, |
|
|
uint8_t |
request, |
|
|
uint8_t |
pwm_period, |
|
|
uint8_t |
pwm_dutycycle |
|
) |
| |
Configure coexistence parameters.
- Parameters
-
| [in] | priority | Coexistence priority threshold. Coexistence priority is toggled if priority is below this value. |
| [in] | request | Coexistence request threshold. Coexistence request is toggled if priority is below this value. |
| [in] | pwm_period | PWM functionality period length in 1ms units |
| [in] | pwm_dutycycle | PWM functionality dutycycle in percentage |
- Returns
- SL_STATUS_OK if successful. Error code otherwise.
◆ sl_bt_coex_set_directional_priority_pulse()
| sl_status_t sl_bt_coex_set_directional_priority_pulse |
( |
uint8_t |
pulse | ) |
|
Set Directional Priority Pulse Width
- Parameters
-
| [in] | pulse | Directional priority pulse width in us |
- Returns
- SL_STATUS_OK if successful. Error code otherwise.
◆ sl_bt_coex_get_counters()
| sl_status_t sl_bt_coex_get_counters |
( |
uint8_t |
reset, |
|
|
size_t |
max_counters_size, |
|
|
size_t * |
counters_len, |
|
|
uint8_t * |
counters |
|
) |
| |
Read coexistence statistic counters from the device. Response contains the list of uint32 type counter values. Counters in the list are in following order: low priority requested, high priority requested, low priority denied, high priority denied, low-priority TX aborted, and high-priority TX aborted. Passing a non-zero value also resets counters.
- Parameters
-
| [in] | reset | Reset counters if parameter value is not zero. |
| [in] | max_counters_size | Size of output buffer passed in counters |
| [out] | counters_len | On return, set to the length of output data written to counters |
| [out] | counters | Coexistence statistic counters |
- Returns
- SL_STATUS_OK if successful. Error code otherwise.