Connection.
Modules | |
| sl_bt_evt_connection_opened | |
| Indicates that a new connection was opened. | |
| sl_bt_evt_connection_parameters | |
| Triggered whenever the connection parameters are changed and at any time a connection is established. | |
| sl_bt_evt_connection_phy_status | |
| Indicates that PHY update procedure is completed. | |
| sl_bt_evt_connection_rssi | |
| Triggered when an connection_get_rssi command has completed. | |
| sl_bt_evt_connection_closed | |
| Indicates that a connection was closed. | |
Enumerations | |
| enum | connection_security_t { connection_mode1_level1 = 0x0, connection_mode1_level2 = 0x1, connection_mode1_level3 = 0x2, connection_mode1_level4 = 0x3 } |
| Security Modes. | |
Functions | |
| sl_status_t | sl_bt_connection_set_default_parameters (uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length) |
| sl_status_t | sl_bt_connection_set_default_preferred_phy (uint8_t preferred_phy, uint8_t accepted_phy) |
| sl_status_t | sl_bt_connection_open (bd_addr address, uint8_t address_type, uint8_t initiating_phy, uint8_t *connection) |
| sl_status_t | sl_bt_connection_set_parameters (uint8_t connection, uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length) |
| sl_status_t | sl_bt_connection_set_preferred_phy (uint8_t connection, uint8_t preferred_phy, uint8_t accepted_phy) |
| sl_status_t | sl_bt_connection_disable_slave_latency (uint8_t connection, uint8_t disable) |
| sl_status_t | sl_bt_connection_get_rssi (uint8_t connection) |
| sl_status_t | sl_bt_connection_read_channel_map (uint8_t connection, size_t max_channel_map_size, size_t *channel_map_len, uint8_t *channel_map) |
| sl_status_t | sl_bt_connection_close (uint8_t connection) |
Connection.
The commands and events in this class are related to managing connection establishment, parameter setting, and disconnection procedures.
Security Modes.
| sl_status_t sl_bt_connection_set_default_parameters | ( | uint16_t | min_interval, |
| uint16_t | max_interval, |
||
| uint16_t | latency, |
||
| uint16_t | timeout, |
||
| uint16_t | min_ce_length, |
||
| uint16_t | max_ce_length |
||
| ) |
Set the default Bluetooth connection parameters. The values are valid for all subsequent connections initiated by this device. To change parameters of an already established connection, use the command sl_bt_connection_set_parameters.
| [in] | min_interval | Minimum value for the connection event interval. This must be set less than or equal to
Default value: 20 ms |
| [in] | max_interval | Maximum value for the connection event interval. This must be set greater than or equal to
Default value: 50 ms |
| [in] | latency | Slave latency, which defines how many connection intervals the slave can skip if it has no data to send
Default value: 0 |
| [in] | timeout | Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.
Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals. Default value: 1000 ms |
| [in] | min_ce_length | Minimum value for the connection event length. This must be set be less than or equal to
Default value: 0x0000 Value is not currently used and is reserved for future. Set to 0. |
| [in] | max_ce_length | Maximum value for the connection event length. This must be set greater than or equal to
Default value: 0xffff |
| sl_status_t sl_bt_connection_set_default_preferred_phy | ( | uint8_t | preferred_phy, |
| uint8_t | accepted_phy |
||
| ) |
Set default preferred and accepted PHYs. PHY settings will be used for all subsequent connections. Non-preferred PHY can also be set if the remote device does not accept any of the preferred PHYs.
The parameter accepted_phy is used to specify PHYs that the stack can accept in a remotely-initiated PHY update request. A PHY update will not happen if none of the accepted PHYs are present in the request.
NOTE: 2M and Coded PHYs are not supported by all devices.
| [in] | preferred_phy | Preferred PHYs. This parameter is a bitfield and multiple PHYs can be set.
Default: 0xff (no preference) |
| [in] | accepted_phy | Accepted PHYs in remotely-initiated PHY update request. This parameter is a bitfield and multiple PHYs can be set.
Default: 0xff (all PHYs accepted) |
| sl_status_t sl_bt_connection_open | ( | bd_addr | address, |
| uint8_t | address_type, |
||
| uint8_t | initiating_phy, |
||
| uint8_t * | connection |
||
| ) |
Connect to an advertising device with the specified initiating PHY on which connectable advertisements on primary advertising channels are received. The Bluetooth stack will enter a state where it continuously scans for the connectable advertising packets from the remote device, which matches the Bluetooth address given as a parameter. Scan parameters set in sl_bt_scanner_set_timing are used in this operation. Upon receiving the advertising packet, the module will send a connection request packet to the target device to initiate a Bluetooth connection. To cancel an ongoing connection process, use sl_bt_connection_close command with the handle received in response from this command.
A connection is opened in no-security mode. If the GATT client needs to read or write the attributes on GATT server requiring encryption or authentication, it must first encrypt the connection using an appropriate authentication method.
If a connection can't be established (for example, the remote device has gone out of range, has entered into deep sleep, or is not advertising), the stack will try to connect forever. In this case, the application will not get an event related to the connection request. To recover from this situation, the application can implement a timeout and call sl_bt_connection_close to cancel the connection request.
This command fails with the connection limit exceeded error if the number of connections attempted exceeds the configured MAX_CONNECTIONS value.
This command fails with the invalid parameter error if the initiating PHY value is invalid or the device does not support PHY.
Later calls of this command have to wait for the ongoing command to complete. A received event sl_bt_evt_connection_opened indicates that the connection opened successfully and a received event sl_bt_evt_connection_closed indicates that connection failures have occurred.
| [in] | address | Address of the device to connect to |
| [in] | address_type | Enum gap_address_type_t. Address type of the device to connect to. Values:
|
| [in] | initiating_phy | Enum gap_phy_type_t. The initiating PHY. Values:
|
| [out] | connection | Handle that will be assigned to the connection after the connection is established. This handle is valid only if the result code of this response is 0 (zero). |
Events
| sl_status_t sl_bt_connection_set_parameters | ( | uint8_t | connection, |
| uint16_t | min_interval, |
||
| uint16_t | max_interval, |
||
| uint16_t | latency, |
||
| uint16_t | timeout, |
||
| uint16_t | min_ce_length, |
||
| uint16_t | max_ce_length |
||
| ) |
Request a change in the connection parameters of a Bluetooth connection.
| [in] | connection | Connection Handle |
| [in] | min_interval | Minimum value for the connection event interval. This must be set less than or equal to max_interval.
|
| [in] | max_interval | Maximum value for the connection event interval. This must be set greater than or equal to min_interval.
|
| [in] | latency | Slave latency, which defines how many connection intervals the slave can skip if it has no data to send
Use 0x0000 for default value |
| [in] | timeout | Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.
Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals. |
| [in] | min_ce_length | Minimum value for the connection event length. This must be set less than or equal to
Value is not currently used and is reserved for future. Set to 0. |
| [in] | max_ce_length | Maximum value for the connection event length. This must be set greater than or equal to
Use 0xffff for no limitation. |
Events
| sl_status_t sl_bt_connection_set_preferred_phy | ( | uint8_t | connection, |
| uint8_t | preferred_phy, |
||
| uint8_t | accepted_phy |
||
| ) |
Sets preferred and accepted PHYs for the given connection. Event sl_bt_evt_connection_phy_status is received when PHY update procedure is completed. Non-preferred PHY can also be set if remote device does not accept any of the preferred PHYs.
The parameter accepted_phy is used for specifying the PHYs that the stack can accept in a remote initiated PHY update request. A PHY update will not occur if none of the accepted PHYs presents in the request.
NOTE: 2M and Coded PHYs are not supported by all devices.
| [in] | connection | Connection handle |
| [in] | preferred_phy | Preferred PHYs. This parameter is a bitfield and multiple PHYs can be set.
Default: 0xff (no preference) |
| [in] | accepted_phy | Accepted PHYs in remotely-initiated PHY update requests. This parameter is a bitfield and multiple PHYs can be set.
Default: 0xff (all PHYs accepted) |
Events
| sl_status_t sl_bt_connection_disable_slave_latency | ( | uint8_t | connection, |
| uint8_t | disable |
||
| ) |
Temporarily enable or disable slave latency. Used only when Bluetooth device is acting as slave. When slave latency is disabled, the slave latency connection parameter is not set to 0 but the device will wake up on every connection interval to receive and send packets.
| [in] | connection | Connection Handle |
| [in] | disable | 0 enable, 1 disable slave latency. Default: 0 |
| sl_status_t sl_bt_connection_get_rssi | ( | uint8_t | connection | ) |
Get the latest RSSI value of a Bluetooth connection. The RSSI value will be reported in a sl_bt_evt_connection_rssi event.
| [in] | connection | Connection handle |
Events
| sl_status_t sl_bt_connection_read_channel_map | ( | uint8_t | connection, |
| size_t | max_channel_map_size, |
||
| size_t * | channel_map_len, |
||
| uint8_t * | channel_map |
||
| ) |
Read channel map for a specified connection.
| [in] | connection | Connection Handle |
| [in] | max_channel_map_size | Size of output buffer passed in channel_map |
| [out] | channel_map_len | On return, set to the length of output data written to channel_map |
| [out] | channel_map | This parameter is 5 bytes and contains 37 1-bit fields. The nth field (in the range 0 to 36) contains the value for the link layer channel index n.
The most significant bits are reserved for future use. |
| sl_status_t sl_bt_connection_close | ( | uint8_t | connection | ) |
Close a Bluetooth connection or cancel an ongoing connection establishment process. The parameter is a connection handle which is reported in sl_bt_evt_connection_opened event or sl_bt_connection_open command response.
| [in] | connection | Handle of the connection to be closed |
Events