Reports any scan request received in advertising mode if the scan request notification is enabled.
Data Structures | |
| struct | sl_bt_evt_advertiser_scan_request_s |
| Data structure of the scan_request event. | |
Macros | |
| #define | sl_bt_evt_advertiser_scan_request_id 0x020400a0 |
| Identifier of the scan_request event. | |
Reports any scan request received in advertising mode if the scan request notification is enabled.
Do not confuse this event with the scan response.
| struct sl_bt_evt_advertiser_scan_request_s |
Data structure of the scan_request event.
| Data Fields | ||
|---|---|---|
| uint8_t | handle |
Advertising set handle where scan request was received |
| bd_addr | address |
Bluetooth address of the scanning device |
| uint8_t | address_type |
Scanner address type. Values:
|
| uint8_t | bonding |
Bonding handle if the remote scanning device has previously bonded with the local device. Values:
|