sl_bt_evt_connection_phy_statusConnection

Indicates that PHY update procedure is completed.

Data Structures

struct  sl_bt_evt_connection_phy_status_s
 Data structure of the phy_status event.
 

Macros

#define sl_bt_evt_connection_phy_status_id   0x040600a0
 Identifier of the phy_status event.
 

Detailed Description

Indicates that PHY update procedure is completed.


Data Structure Documentation

◆ sl_bt_evt_connection_phy_status_s

struct sl_bt_evt_connection_phy_status_s

Data structure of the phy_status event.

Data Fields
uint8_t connection

Connection handle

uint8_t phy

Current active PHY. See values from sl_bt_connection_set_preferred_phy command.