IQ sample report from connectionless CTE packets.
Data Structures | |
struct | sl_bt_evt_cte_receiver_connectionless_iq_report_s |
Data structure of the connectionless_iq_report event. | |
Macros | |
#define | sl_bt_evt_cte_receiver_connectionless_iq_report_id 0x014500a0 |
Identifier of the connectionless_iq_report event. | |
IQ sample report from connectionless CTE packets.
struct sl_bt_evt_cte_receiver_connectionless_iq_report_s |
Data structure of the connectionless_iq_report event.
Data Fields | ||
---|---|---|
uint16_t | status |
Status of CTE IQ sampling |
uint16_t | sync |
Periodic advertising synchronization handle |
uint8_t | channel |
The channel on which the CTE packet was received |
int8_t | rssi |
RSSI in the received CTE packet. Unit: dBm |
uint8_t | rssi_antenna_id |
The ID of the antenna on which RSSI was measured |
uint8_t | cte_type |
The CTE type
|
uint8_t | slot_durations |
Slot durations
|
uint16_t | event_counter |
The event counter of the periodic advertising train |
uint8array | samples |
IQ samples of the received CTE packet. I and Q samples follow each other alternately (I, Q, I, Q, ...) |