IQ sample report from DTM CTE packets.
Data Structures | |
| struct | sl_bt_evt_cte_receiver_dtm_iq_report_s |
| Data structure of the dtm_iq_report event. | |
Macros | |
| #define | sl_bt_evt_cte_receiver_dtm_iq_report_id 0x024500a0 |
| Identifier of the dtm_iq_report event. | |
IQ sample report from DTM CTE packets.
| struct sl_bt_evt_cte_receiver_dtm_iq_report_s |
Data structure of the dtm_iq_report event.
| Data Fields | ||
|---|---|---|
| uint16_t | status |
Status of CTE IQ sampling |
| uint8_t | channel |
The channel on which the CTE packet was received |
| int8_t | rssi |
RSSI in the received CTE packet. Unit: dBm |
| uint8_t | rssi_antenna_id |
The ID of the antenna on which RSSI was measured |
| uint8_t | cte_type |
The CTE type
|
| uint8_t | slot_durations |
Slot durations
|
| uint16_t | event_counter |
The event counter of the periodic advertising train or the connection |
| uint8array | samples |
IQ samples of the received CTE packet. I and Q samples follow each other alternately (I, Q, I, Q, ...) |