IQ samples report from Silicon Labs CTE packets.
Data Structures | |
| struct | sl_bt_evt_cte_receiver_silabs_iq_report_s |
| Data structure of the silabs_iq_report event. | |
Macros | |
| #define | sl_bt_evt_cte_receiver_silabs_iq_report_id 0x034500a0 |
| Identifier of the silabs_iq_report event. | |
IQ samples report from Silicon Labs CTE packets.
| struct sl_bt_evt_cte_receiver_silabs_iq_report_s |
Data structure of the silabs_iq_report event.
| Data Fields | ||
|---|---|---|
| uint16_t | status |
Status of CTE IQ sampling |
| bd_addr | address |
Bluetooth address of the remote device |
| uint8_t | address_type |
Advertiser address type. Values:
|
| uint8_t | phy |
The PHY on which the packet is received.
|
| uint8_t | channel |
The channel on which the CTE packet was received |
| int8_t | rssi |
RSSI in the received CTE packet. Unit: dBm |
| uint8_t | rssi_antenna_id |
The ID of the antenna on which RSSI was measured |
| uint8_t | cte_type |
The CTE type
|
| uint8_t | slot_durations |
Slot durations
|
| uint16_t | packet_counter |
The event counter of the periodic advertising train or the connection |
| uint8array | samples |
IQ samples of the received CTE packet. I and Q samples follow each other alternately (I, Q, I, Q, ...) |