Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.
Data Structures | |
| struct | sl_bt_evt_gatt_descriptor_s |
| Data structure of the descriptor event. | |
Macros | |
| #define | sl_bt_evt_gatt_descriptor_id 0x030900a0 |
| Identifier of the descriptor event. | |
Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.
It is generated after issuing the sl_bt_gatt_discover_descriptors command.
| struct sl_bt_evt_gatt_descriptor_s |
Data structure of the descriptor event.
| Data Fields | ||
|---|---|---|
| uint8_t | connection |
Connection handle |
| uint16_t | descriptor |
GATT characteristic descriptor handle |
| uint8array | uuid |
Descriptor UUID in little endian format |