Indicates that the current GATT procedure was completed successfully or that it failed with an error.
Data Structures | |
| struct | sl_bt_evt_gatt_procedure_completed_s |
| Data structure of the procedure_completed event. | |
Macros | |
| #define | sl_bt_evt_gatt_procedure_completed_id 0x060900a0 |
| Identifier of the procedure_completed event. | |
Indicates that the current GATT procedure was completed successfully or that it failed with an error.
All GATT commands excluding sl_bt_gatt_write_characteristic_value_without_response and sl_bt_gatt_send_characteristic_confirmation will trigger this event. As a result, the application must wait for this event before issuing another GATT command (excluding the two aforementioned exceptions).