Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.
Data Structures | |
struct | sl_bt_evt_gatt_server_attribute_value_s |
Data structure of the attribute_value event. | |
Macros | |
#define | sl_bt_evt_gatt_server_attribute_value_id 0x000a00a0 |
Identifier of the attribute_value event. | |
Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.
The parameter att_opcode
describes which GATT procedure was used to change the value.
struct sl_bt_evt_gatt_server_attribute_value_s |
Data structure of the attribute_value event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Connection handle |
uint16_t | attribute |
Attribute Handle |
uint8_t | att_opcode |
Enum gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received. |
uint16_t | offset |
Value offset |
uint8array | value |
Value |