Indicates that a remote GATT client is attempting to read a value of an attribute from the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
Data Structures | |
| struct | sl_bt_evt_gatt_server_user_read_request_s |
| Data structure of the user_read_request event. | |
Macros | |
| #define | sl_bt_evt_gatt_server_user_read_request_id 0x010a00a0 |
| Identifier of the user_read_request event. | |
Indicates that a remote GATT client is attempting to read a value of an attribute from the local GATT database, where the attribute was defined in the GATT database XML file to have the type="user".
The parameter att_opcode informs which GATT procedure was used to read the value. The application needs to respond to this request by using the sl_bt_gatt_server_send_user_read_response command within 30 seconds, otherwise further GATT transactions are not allowed by the remote side.
| struct sl_bt_evt_gatt_server_user_read_request_s |
Data structure of the user_read_request event.
| Data Fields | ||
|---|---|---|
| uint8_t | connection |
Connection handle |
| uint16_t | characteristic |
GATT characteristic handle. This value is normally received from the gatt_characteristic event. |
| uint8_t | att_opcode |
Enum gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received. |
| uint16_t | offset |
Value offset |