Indicate that a GATT service in the remote GATT database was discovered.
Data Structures | |
struct | sl_bt_evt_gatt_service_s |
Data structure of the service event. | |
Macros | |
#define | sl_bt_evt_gatt_service_id 0x010900a0 |
Identifier of the service event. | |
Indicate that a GATT service in the remote GATT database was discovered.
This event is generated after issuing either the sl_bt_gatt_discover_primary_services or sl_bt_gatt_discover_primary_services_by_uuid command.
struct sl_bt_evt_gatt_service_s |
Data structure of the service event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Connection handle |
uint32_t | service |
GATT service handle |
uint8array | uuid |
Service UUID in little endian format |