Reports an advertising or scan response packet that is received by the device's radio while in scanning mode.
Data Structures | |
| struct | sl_bt_evt_scanner_scan_report_s |
| Data structure of the scan_report event. | |
Macros | |
| #define | sl_bt_evt_scanner_scan_report_id 0x010500a0 |
| Identifier of the scan_report event. | |
Reports an advertising or scan response packet that is received by the device's radio while in scanning mode.
| struct sl_bt_evt_scanner_scan_report_s |
Data structure of the scan_report event.
| Data Fields | ||
|---|---|---|
| uint8_t | packet_type |
Bits 0..2 : advertising packet type
Bits 3..4 : Reserved for future Bits 5..6 : data completeness
Bit 7 : legacy or extended advertising
|
| bd_addr | address |
Bluetooth address of the remote device |
| uint8_t | address_type |
Advertiser address type. Values:
|
| uint8_t | bonding |
Bonding handle if the remote advertising device has previously bonded with the local device. Values:
|
| uint8_t | primary_phy |
Enum gap_phy_type_t. The PHY on which advertising packets are transmitted on the primary advertising channel. Values:
|
| uint8_t | secondary_phy |
Enum gap_phy_type_t. The PHY on which advertising packets are transmitted on the secondary advertising channel. Values:
|
| uint8_t | adv_sid |
Advertising set identifier |
| int8_t | tx_power |
TX power value in the received packet header. Units: dBm
|
| int8_t | rssi |
Signal strength indicator (RSSI) in the last received packet. Units: dBm
|
| uint8_t | channel |
The channel number on which the last packet was received |
| uint16_t | periodic_interval |
The periodic advertising interval. Value 0 indicates no periodic advertising. Otherwise,
|
| uint8array | data |
Advertising or scan response data |