Indicates that a periodic advertising synchronization has been opened.
Data Structures | |
| struct | sl_bt_evt_sync_opened_s |
| Data structure of the opened event. | |
Macros | |
| #define | sl_bt_evt_sync_opened_id 0x004200a0 |
| Identifier of the opened event. | |
Indicates that a periodic advertising synchronization has been opened.
| struct sl_bt_evt_sync_opened_s |
Data structure of the opened event.
| Data Fields | ||
|---|---|---|
| uint16_t | sync |
Periodic advertising synchronization handle |
| uint8_t | adv_sid |
Advertising set identifier |
| bd_addr | address |
Address of the advertiser |
| uint8_t | address_type |
Advertiser address type. Values:
|
| uint8_t | adv_phy |
Enum gap_phy_type_t. The advertiser PHY. Values:
|
| uint16_t | adv_interval |
The periodic advertising interval. Value in units of 1.25 ms
|
| uint16_t | clock_accuracy |
Enum sync_advertiser_clock_accuracy_t. The advertiser clock accuracy. |
| uint8_t | bonding |
Bonding handle. Values:
|