Security Manager.
Modules | |
| sl_bt_evt_sm_passkey_display | |
| Indicates a request to display the passkey to the user. | |
| sl_bt_evt_sm_passkey_request | |
| Indicates a request for the passkey prompt displayed on the remote device. | |
| sl_bt_evt_sm_confirm_passkey | |
| Indicates a request for passkey display and confirmation by the user. | |
| sl_bt_evt_sm_bonded | |
| Triggered after the pairing or bonding procedure is successfully completed. | |
| sl_bt_evt_sm_bonding_failed | |
| This event is triggered if the pairing or bonding procedure fails. | |
| sl_bt_evt_sm_confirm_bonding | |
| Indicates a user request to display that the new bonding request is received and for the user to confirm the request. | |
| sl_bt_evt_sm_list_bonding_entry | |
| Triggered by the command sl_bt_sm_list_all_bondings if bondings exist in the local database. | |
| sl_bt_evt_sm_list_all_bondings_complete | |
| Triggered by the sl_bt_sm_list_all_bondings and follows sl_bt_evt_sm_list_bonding_entry events. | |
Enumerations | |
| enum | sm_bonding_key_t { sm_bonding_key_ltk = 0x1, sm_bonding_key_addr_public = 0x2, sm_bonding_key_addr_static = 0x4, sm_bonding_key_irk = 0x8, sm_bonding_key_edivrand = 0x10, sm_bonding_key_csrk = 0x20, sm_bonding_key_masterid = 0x40 } |
| Bonding Keys. | |
| enum | sm_io_capability_t { sm_io_capability_displayonly = 0x0, sm_io_capability_displayyesno = 0x1, sm_io_capability_keyboardonly = 0x2, sm_io_capability_noinputnooutput = 0x3, sm_io_capability_keyboarddisplay = 0x4 } |
| SMP I/O Capabilities. | |
Functions | |
| sl_status_t | sl_bt_sm_configure (uint8_t flags, uint8_t io_capabilities) |
| sl_status_t | sl_bt_sm_set_minimum_key_size (uint8_t minimum_key_size) |
| sl_status_t | sl_bt_sm_set_debug_mode () |
| sl_status_t | sl_bt_sm_add_to_whitelist (bd_addr address, uint8_t address_type) |
| sl_status_t | sl_bt_sm_store_bonding_configuration (uint8_t max_bonding_count, uint8_t policy_flags) |
| sl_status_t | sl_bt_sm_set_bondable_mode (uint8_t bondable) |
| sl_status_t | sl_bt_sm_set_passkey (int32_t passkey) |
| sl_status_t | sl_bt_sm_set_oob_data (size_t oob_data_len, const uint8_t *oob_data) |
| sl_status_t | sl_bt_sm_use_sc_oob (uint8_t enable, size_t max_oob_data_size, size_t *oob_data_len, uint8_t *oob_data) |
| sl_status_t | sl_bt_sm_set_sc_remote_oob_data (size_t oob_data_len, const uint8_t *oob_data) |
| sl_status_t | sl_bt_sm_increase_security (uint8_t connection) |
| sl_status_t | sl_bt_sm_enter_passkey (uint8_t connection, int32_t passkey) |
| sl_status_t | sl_bt_sm_passkey_confirm (uint8_t connection, uint8_t confirm) |
| sl_status_t | sl_bt_sm_bonding_confirm (uint8_t connection, uint8_t confirm) |
| sl_status_t | sl_bt_sm_list_all_bondings () |
| sl_status_t | sl_bt_sm_delete_bonding (uint8_t bonding) |
| sl_status_t | sl_bt_sm_delete_bondings () |
Security Manager.
The commands in this class manage Bluetooth security, including commands for starting and stopping encryption and commands for management of all bonding operations.
The following procedure is used to bond with a remote device:
The following procedure can be used to respond to the bonding initiated by a remote device:
If MITM is required, the application needs to display or ask the user to enter a passkey during the process. See events sl_bt_evt_sm_passkey_display and sl_bt_evt_sm_passkey_request for more information.
| enum sm_bonding_key_t |
Bonding Keys.
| enum sm_io_capability_t |
SMP I/O Capabilities.
| sl_status_t sl_bt_sm_configure | ( | uint8_t | flags, |
| uint8_t | io_capabilities |
||
| ) |
Configure security requirements and I/O capabilities of the system.
| [in] | flags | Security requirement bitmask. Bit 0:
Bit 1:
Bit 2:
Bit 3:
Bit 4:
Bit 5 to 7: Reserved Default value: 0x00 |
| [in] | io_capabilities | Enum sm_io_capability_t. I/O Capabilities. The default I/O Capability used by the stack is No Input and No Output. Values:
|
| sl_status_t sl_bt_sm_set_minimum_key_size | ( | uint8_t | minimum_key_size | ) |
Set the minimum allowed key size used for bonding. The default value is 16 bytes.
| [in] | minimum_key_size | Minimum allowed key size for bonding. Range: 7 to 16 |
| sl_status_t sl_bt_sm_set_debug_mode | ( | | ) |
Set Security Manager in debug mode. In this mode, the secure connections bonding uses known debug keys, so that the encrypted packet can be opened by Bluetooth protocol analyzer. To disable the debug mode, restart the device.
Bondings made in debug mode are unsecure.
| sl_status_t sl_bt_sm_add_to_whitelist | ( | bd_addr | address, |
| uint8_t | address_type |
||
| ) |
Add device to whitelist, which can be enabled with sl_bt_gap_enable_whitelisting.
| [in] | address | Address of the device added to whitelist |
| [in] | address_type | Enum gap_address_type_t. Address type of the device added to whitelist. Values:
|
| sl_status_t sl_bt_sm_store_bonding_configuration | ( | uint8_t | max_bonding_count, |
| uint8_t | policy_flags |
||
| ) |
Set the maximum allowed bonding count and bonding policy. The maximum number of bondings that can be supported depends on how much user data is stored in the NVM and the NVM size. When bond policy value 1 or 2 is selected the stack will automatically write the new bond, as per the policy, only if the maximum allowed bonding count has been reached. If the stack is not able to write a new bond for any other reason (e.g. nvm full) then an error will be thrown through the bonding_failed event indicating why the bonding could not be written. It is left up to the application to manually release space from the nvm (e.g. by deleting one of the existing bonds or application data) so that a new bond can be saved. The default value is 13.
| [in] | max_bonding_count | Maximum allowed bonding count. Range: 1 to 32 |
| [in] | policy_flags | Bonding policy. Values:
Default: 0 |
| sl_status_t sl_bt_sm_set_bondable_mode | ( | uint8_t | bondable | ) |
Set whether the device should accept new bondings. By default, the device does not accept new bondings.
| [in] | bondable | Bondable mode. Values:
Default value: 0 |
| sl_status_t sl_bt_sm_set_passkey | ( | int32_t | passkey | ) |
Enter a fixed passkey, which will be used in the sl_bt_evt_sm_passkey_display event.
| [in] | passkey | Passkey. Valid range: 0-999999. Set -1 to disable and start using random passkeys. |
| sl_status_t sl_bt_sm_set_oob_data | ( | size_t | oob_data_len, |
| const uint8_t * | oob_data |
||
| ) |
Set OOB data (out-of-band encryption data) for legacy pairing for a device. OOB data may be, for example, a PIN code exchanged over an alternate path, such as NFC. The device will not allow any other bonding if OOB data is set. OOB data can't be set simultaneously with secure connections OOB data.
| [in] | oob_data_len | Array length |
| [in] | oob_data | OOB data. To set OOB data, send a 16-byte array. To clear OOB data, send a zero-length array. |
| sl_status_t sl_bt_sm_use_sc_oob | ( | uint8_t | enable, |
| size_t | max_oob_data_size, |
||
| size_t * | oob_data_len, |
||
| uint8_t * | oob_data |
||
| ) |
Enable the use of OOB data (out-of-band encryption data) for a device for secure connections pairing. Enabling will generate new OOB data and confirm values, which can be sent to the remote device. After enabling the secure connections OOB data, the remote devices OOB data can be set with sl_bt_sm_set_sc_remote_oob_data. Calling this function will erase any set remote device OOB data and confirm values. The device will not allow any other bonding if OOB data is set. The secure connections OOB data cannot be enabled simultaneously with legacy pairing OOB data.
| [in] | enable | Enable OOB with secure connections pairing. Values:
|
| [in] | max_oob_data_size | Size of output buffer passed in oob_data |
| [out] | oob_data_len | On return, set to the length of output data written to oob_data |
| [out] | oob_data | OOB data. 32-byte array. The first 16-bytes contain randomly-generated OOB data and the last 16-bytes confirm value. |
| sl_status_t sl_bt_sm_set_sc_remote_oob_data | ( | size_t | oob_data_len, |
| const uint8_t * | oob_data |
||
| ) |
Set OOB data and confirm values (out-of-band encryption) received from the remote device for secure connections pairing. OOB data must be enabled with sl_bt_sm_use_sc_oob before setting the remote device OOB data.
| [in] | oob_data_len | Array length |
| [in] | oob_data | Remote device OOB data and confirm values. To set OOB data, send a 32-byte array. First 16-bytes is OOB data and last 16-bytes the confirm value. To clear OOB data, send a zero-length array. |
| sl_status_t sl_bt_sm_increase_security | ( | uint8_t | connection | ) |
Enhance the security of a connection to current security requirements. On an unencrypted connection, it will encrypt the connection and will also perform bonding if requested by both devices. On an encrypted connection, it will cause the connection to be re-encrypted.
| [in] | connection | Connection handle |
Events
| sl_status_t sl_bt_sm_enter_passkey | ( | uint8_t | connection, |
| int32_t | passkey |
||
| ) |
Enter a passkey after receiving a passkey request event.
| [in] | connection | Connection handle |
| [in] | passkey | Passkey. Valid range: 0-999999. Set -1 to cancel pairing. |
| sl_status_t sl_bt_sm_passkey_confirm | ( | uint8_t | connection, |
| uint8_t | confirm |
||
| ) |
Accept or reject the reported passkey confirm value.
| [in] | connection | Connection handle |
| [in] | confirm | Acceptance. Values:
|
| sl_status_t sl_bt_sm_bonding_confirm | ( | uint8_t | connection, |
| uint8_t | confirm |
||
| ) |
Accept or reject the bonding request.
| [in] | connection | Connection handle |
| [in] | confirm | Acceptance. Values:
|
| sl_status_t sl_bt_sm_list_all_bondings | ( | | ) |
List all bondings stored in the bonding database. Bondings are reported by the sl_bt_evt_sm_list_bonding_entry event for each bonding and the report is ended with sl_bt_evt_sm_list_all_bondings_complete event. Use only for debugging purposes because reading from the persistent store is relatively slow.
Events
| sl_status_t sl_bt_sm_delete_bonding | ( | uint8_t | bonding | ) |
Delete specified bonding information or whitelist from the persistent store.
| [in] | bonding | Bonding handle |
| sl_status_t sl_bt_sm_delete_bondings | ( | | ) |
Delete all bonding information and whitelist from the persistent store.