Synchronization.
Modules | |
| sl_bt_evt_sync_opened | |
| Indicates that a periodic advertising synchronization has been opened. | |
| sl_bt_evt_sync_data | |
| Reports a received periodic advertisement packet. | |
| sl_bt_evt_sync_closed | |
| Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled. | |
Enumerations | |
| enum | sync_advertiser_clock_accuracy_t { sync_clock_accuracy_500 = 0x500, sync_clock_accuracy_250 = 0x250, sync_clock_accuracy_150 = 0x150, sync_clock_accuracy_100 = 0x100, sync_clock_accuracy_75 = 0x75, sync_clock_accuracy_50 = 0x50, sync_clock_accuracy_30 = 0x30, sync_clock_accuracy_20 = 0x20 } |
| Advertiser Clock Accuracy. | |
Functions | |
| sl_status_t | sl_bt_sync_set_parameters (uint16_t skip, uint16_t timeout, uint32_t flags) |
| sl_status_t | sl_bt_sync_open (bd_addr address, uint8_t address_type, uint8_t adv_sid, uint16_t *sync) |
| sl_status_t | sl_bt_sync_close (uint16_t sync) |
Synchronization.
Provides periodic advertising synchronization feature.
Advertiser Clock Accuracy.
| sl_status_t sl_bt_sync_set_parameters | ( | uint16_t | skip, |
| uint16_t | timeout, |
||
| uint32_t | flags |
||
| ) |
Configure periodic advertiser synchronization parameters. The specified parameters take effect immediately for all advertisers that have not already established synchronization.
The application should determine skip and timeout values based on the periodic advertising interval provided by the advertiser. If skip and timeout are used, select appropriate values so that they allow a few receiving attempts. Periodic advertising intervals are reported in event sl_bt_evt_scanner_scan_report.
| [in] | skip | The maximum number of periodic advertising packets that can be skipped after a successful receive.
|
| [in] | timeout | The maximum permitted time between successful receives. If this time is exceeded, synchronization is lost. Unit: 10 ms.
|
| [in] | flags | No flags defined currently |
| sl_status_t sl_bt_sync_open | ( | bd_addr | address, |
| uint8_t | address_type, |
||
| uint8_t | adv_sid, |
||
| uint16_t * | sync |
||
| ) |
Start establishing synchronization with the specified periodic advertiser in parallel with other advertisers given in previous invocations of this command. The stack will internally enable scanning when needed so that synchronizations can occur. The scanning responses from the internal scanning are not passed to the application unless the application has also enabled scanning.
Advertisers that have not already synced before the invocation of this command will be synced using the skip and timeout values configured in the most recent invocation of command sl_bt_evt_scanner_scan_report.
| [in] | address | Address of the advertiser |
| [in] | address_type | Advertiser address type. Values:
|
| [in] | adv_sid | Advertising set identifier |
| [out] | sync | A handle that will be assigned to the periodic advertising synchronization after the synchronization is established. This handle is valid only if the result code of this response is SL_STATUS_OK. |
Events
| sl_status_t sl_bt_sync_close | ( | uint16_t | sync | ) |
Closes a periodic advertising synchronization or cancels an ongoing attempt of establishing a synchronization.
| [in] | sync | Periodic advertising synchronization handle |
Events