Silicon Labs
bluetooth/3.0/~/structsl-bt-rsp-connection-set-default-parameters-s
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
    Results 1-5 of 5 for bluetooth/3.0/~/structsl-bt-rsp-connection-set-default-parameters-s in 0.17 seconds
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    // Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System ... sl_bt_rsp_system_set_identity_address_id 0x13010020 ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
    Connection | Bluetooth Stack API Reference | Bluetooth LE | v8.1.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-connect...
    8.1.0 Connection# Connection. ... sl_bt_rsp_connection_set_default_parameters_id 0x00060020 ... Set the supervision timeout at a value which allows communication attempts over at least a few ...
    System | Bluetooth API Reference Guide | Bluetooth LE | v6.0.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-sys...
    // Bluetooth LE//Version 6.0.0 //Bluetooth API Reference Guide //System ... sl_bt_rsp_system_set_identity_address_id 0x13010020 ... Bluetooth identity address in little endian format
    Resource TypeSoftware API Documentation
    GATT Server | GATT Server | Bluetooth LE | v3.2 | Silicon Labs
    https://docs.silabs.com/....
    Set the maximum size of ATT Message Transfer Units (MTU). ... Volume 3, Part G, 4.9.5). Parameters [in]| `connection`| Connection handle ... Value 0 sets the default database capabilities.
    Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
    https://docs.silabs.com/.../sl-bt-adverti...
    // Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... sl_bt_rsp_advertiser_clear_random_address_id 0x11040020 ... Time range: 10 ms to 655.35 s Default : 0 uint8_t
      Results 1-5 of 5 for bluetooth/3.0/~/structsl-bt-rsp-connection-set-default-parameters-s