sl_bt_rsp_system_linklayer_configure_id 0x0e010020 ... To boot into a DFU mode on series 2, use the Bootloader API bootloader_ ... Bluetooth identity address in little endian format
sl_bt_rsp_system_linklayer_configure_id 0x0e010020 ... To boot into a DFU mode on series 2, use the Bootloader API bootloader_ ... Bluetooth identity address in little endian format
sl_bt_evt_gatt_server_attribute_value Indicates that the value of an attribute in the local GATT database was ... sl_bt_evt_gatt_server_user_read_request Indicates that a remote GATT client is ...
sl_bt_rsp_connection_set_remote_power_reporting_id 0x0a060020 ... To recover from this situation, the application can implement a timeout and call sl_bt_connection_close to cancel the ...
// Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... To enhance the privacy, the application should schedule periodic address updates by calling this command ...
Results 1-5 of 5 for bluetooth/3.0/~/structsl-bt-rsp-user-message-to-target-s