GAP#
GAP.
Enumerations | |
|---|---|
enum | sl_bt_gap_address_type_t { sl_bt_gap_public_address = 0x0, sl_bt_gap_static_address = 0x1, sl_bt_gap_random_resolvable_address = 0x2, sl_bt_gap_random_nonresolvable_address = 0x3 } |
Device Address Types. | |
enum | sl_bt_gap_phy_type_t { sl_bt_gap_1m_phy = 0x1, sl_bt_gap_2m_phy = 0x2, sl_bt_gap_coded_phy = 0x4, sl_bt_gap_any_phys = 0xff } |
PHY Types. | |
enum | sl_bt_gap_phy_and_coding_type_t { sl_bt_gap_1m_phy_uncoded = 0x1, sl_bt_gap_2m_phy_uncoded = 0x2, sl_bt_gap_coded_phy_125k = 0x4, sl_bt_gap_coded_phy_500k = 0x8 } |
PHY Types with Coding Schemes. | |
Functions | |
|---|---|
sl_status_t | sl_bt_gap_set_privacy_mode (uint8_t privacy, uint8_t interval) |
sl_status_t | sl_bt_gap_set_data_channel_classification (size_t channel_map_len, const uint8_t *channel_map) |
sl_status_t | sl_bt_gap_enable_whitelisting (uint8_t enable) |
Detailed Description#
GAP.
The commands and events in this class are related to the Generic Access Profile (GAP) in Bluetooth.
Enumeration Type Documentation#
sl_bt_gap_address_type_t#
Device Address Types.
Enumerator | |
|---|---|
sl_bt_gap_public_address | (0x0) Public device address |
sl_bt_gap_static_address | (0x1) Static device address |
sl_bt_gap_random_resolvable_address | (0x2) Private resolvable random address |
sl_bt_gap_random_nonresolvable_address | (0x3) Private non-resolvable random address |
sl_bt_gap_phy_type_t#
enum sl_bt_gap_phy_type_t
PHY Types.
Enumerator | |
|---|---|
sl_bt_gap_1m_phy | (0x1) 1M PHY |
sl_bt_gap_2m_phy | (0x2) 2M PHY |
sl_bt_gap_coded_phy | (0x4) Coded PHY, 125k (S=8) or 500k (S=2) |
sl_bt_gap_any_phys | (0xff) Any PHYs the device supports |
sl_bt_gap_phy_and_coding_type_t#
PHY Types with Coding Schemes.
Enumerator | |
|---|---|
sl_bt_gap_1m_phy_uncoded | (0x1) 1M PHY |
sl_bt_gap_2m_phy_uncoded | (0x2) 2M PHY |
sl_bt_gap_coded_phy_125k | (0x4) 125k Coded PHY (S=8) |
sl_bt_gap_coded_phy_500k | (0x8) 500k Coded PHY (S=2) |
Function Documentation#
sl_bt_gap_set_privacy_mode()#
sl_status_t sl_bt_gap_set_privacy_mode | ( | uint8_t |
|
uint8_t |
| ||
) |
Enable or disable the privacy feature on all GAP roles. New privacy mode will take effect for advertising next time advertising is enabled, for scanning next time scanning is enabled, and for initiating on the next open connection command. When privacy is enabled and the device is advertising or scanning, the stack will maintain a periodic timer with the specified time interval as a timeout value. At each timeout, the stack will generate a new private resolvable address and use it in advertising data packets and scanning requests.
By default, privacy feature is disabled.
Parameters
[in] |
| Values:
|
[in] |
| The minimum time interval between a private address change. This parameter is ignored if this command is issued to disable privacy mode. Values:
|
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_gap_set_data_channel_classification()#
sl_status_t sl_bt_gap_set_data_channel_classification | ( | size_t |
|
const uint8_t * |
| ||
) |
Specify a channel classification for data channels. This classification persists until overwritten with a subsequent command or until the system is reset.
Parameters
[in] |
| Array length |
[in] |
| This parameter is 5 bytes and contains 37 1-bit fields. The nth field (in the range 0 to 36) contains the value for the link layer channel index n.
The rest of most significant bits are reserved for future use and must be set to 0. At least two channels shall be marked as unknown. |
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_gap_enable_whitelisting()#
sl_status_t sl_bt_gap_enable_whitelisting ( uint8_t
enable)
Enable or disable whitelisting. The setting will be effective the next time that scanning is enabled. To add devices to the whitelist, either bond with the device or add it manually with sl_bt_sm_add_to_whitelist.
Parameters
[in] |
| 1 enable, 0 disable whitelisting. |
Returns
SL_STATUS_OK if successful. Error code otherwise.