sl_bt_evt_connection_get_remote_tx_power_completedConnection
Indicates that reading remote transmit power initiated by sl_bt_connection_get_remote_tx_power command has completed.
Data Structures | |
struct | sl_bt_evt_connection_get_remote_tx_power_completed_s |
Data structure of the get_remote_tx_power_completed event. | |
Macros | |
#define | sl_bt_evt_connection_get_remote_tx_power_completed_id 0x050600a0 |
Identifier of the get_remote_tx_power_completed event. | |
Detailed Description
Indicates that reading remote transmit power initiated by sl_bt_connection_get_remote_tx_power command has completed.
Data Structure Documentation
◆ sl_bt_evt_connection_get_remote_tx_power_completed_s
struct sl_bt_evt_connection_get_remote_tx_power_completed_s |
Data structure of the get_remote_tx_power_completed event.
Data Fields | ||
---|---|---|
uint16_t | status |
SL_STATUS_OK or another error code indicating the reading remote transmit power operation failed. |
uint8_t | connection |
Handle of the connection |
uint8_t | phy |
Enum sl_bt_gap_phy_and_coding_type_t. The PHY for which the transmit power is reported. Values:
|
int8_t | power_level |
Transmit power level. Values:
|
uint8_t | flags |
Enum sl_bt_connection_tx_power_flag_t. Transmit power level flags. Ignore this field if
|
int8_t | delta |
Change in transmit power level. Values:
|