sl_bt_evt_connection_tx_powerConnection
Reports a transmit power change on the local device of a connection if transmit power reporting has been enabled.
Data Structures | |
struct | sl_bt_evt_connection_tx_power_s |
Data structure of the tx_power event. | |
Macros | |
#define | sl_bt_evt_connection_tx_power_id 0x060600a0 |
Identifier of the tx_power event. | |
Detailed Description
Reports a transmit power change on the local device of a connection if transmit power reporting has been enabled.
Enable or disable transmit power reporting using sl_bt_connection_set_power_reporting command.
Data Structure Documentation
◆ sl_bt_evt_connection_tx_power_s
struct sl_bt_evt_connection_tx_power_s |
Data structure of the tx_power event.
Data Fields | ||
---|---|---|
uint8_t | connection |
Handle of the connection |
uint8_t | phy |
Enum sl_bt_gap_phy_and_coding_type_t. The PHY which the transmit power is reported for. Values:
|
int8_t | power_level |
Transmit power level. Values:
|
uint8_t | flags |
Enum sl_bt_connection_tx_power_flag_t. Transmit power level flags. Ignore this field if
|
int8_t | delta |
Change in transmit power level. Values:
|