sl_bt_evt_dfu_bootDevice Firmware Update

This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).

Data Structures

struct  sl_bt_evt_dfu_boot_s
 Data structure of the boot event.
 

Macros

#define sl_bt_evt_dfu_boot_id   0x000000a0
 Identifier of the boot event.
 

Detailed Description

This event indicates that the device booted in DFU mode and is now ready to receive commands related to device firmware upgrade (DFU).


Data Structure Documentation

◆ sl_bt_evt_dfu_boot_s

struct sl_bt_evt_dfu_boot_s

Data structure of the boot event.

Data Fields
uint32_t version

The version of the bootloader