sl_bt_evt_gatt_descriptorGATT Client

Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.

Data Structures

struct  sl_bt_evt_gatt_descriptor_s
 Data structure of the descriptor event.
 

Macros

#define sl_bt_evt_gatt_descriptor_id   0x030900a0
 Identifier of the descriptor event.
 

Detailed Description

Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.

It is generated after issuing the sl_bt_gatt_discover_descriptors command.


Data Structure Documentation

◆ sl_bt_evt_gatt_descriptor_s

struct sl_bt_evt_gatt_descriptor_s

Data structure of the descriptor event.

Data Fields
uint8_t connection

Connection handle

uint16_t descriptor

GATT characteristic descriptor handle

uint8array uuid

Descriptor UUID in little endian format