sl_bt_evt_sm_list_bonding_entrySecurity Manager

Triggered by the command sl_bt_sm_list_all_bondings if bondings exist in the local database.

Data Structures

struct  sl_bt_evt_sm_list_bonding_entry_s
 Data structure of the list_bonding_entry event.
 

Macros

#define sl_bt_evt_sm_list_bonding_entry_id   0x050f00a0
 Identifier of the list_bonding_entry event.
 

Detailed Description

Triggered by the command sl_bt_sm_list_all_bondings if bondings exist in the local database.


Data Structure Documentation

◆ sl_bt_evt_sm_list_bonding_entry_s

struct sl_bt_evt_sm_list_bonding_entry_s

Data structure of the list_bonding_entry event.

Data Fields
uint8_t bonding

Bonding handle

bd_addr address

Bluetooth address of the remote device

uint8_t address_type

Enum sl_bt_gap_address_type_t. Address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address
  • sl_bt_gap_static_address (0x1): Static device address