sl_bt_evt_sync_dataSynchronization
Reports a received periodic advertisement packet.
Data Structures | |
struct | sl_bt_evt_sync_data_s |
Data structure of the data event. | |
Macros | |
#define | sl_bt_evt_sync_data_id 0x024200a0 |
Identifier of the data event. | |
Detailed Description
Reports a received periodic advertisement packet.
Data Structure Documentation
◆ sl_bt_evt_sync_data_s
struct sl_bt_evt_sync_data_s |
Data structure of the data event.
Data Fields | ||
---|---|---|
uint16_t | sync |
Periodic advertising synchronization handle |
int8_t | tx_power |
TX power value in the received packet header. Units: dBm
|
int8_t | rssi |
Signal strength indicator (RSSI) in the latest received packet. Units: dBm
|
uint8_t | data_status |
Data completeness:
|
uint8array | data |
Periodic advertising data |