sl_bt_evt_system_hardware_errorSystem

Indicates that a hardware-related error has occurred.

Data Structures

struct  sl_bt_evt_system_hardware_error_s
 Data structure of the hardware_error event.
 

Macros

#define sl_bt_evt_system_hardware_error_id   0x050100a0
 Identifier of the hardware_error event.
 

Detailed Description

Indicates that a hardware-related error has occurred.


Data Structure Documentation

◆ sl_bt_evt_system_hardware_error_s

struct sl_bt_evt_system_hardware_error_s

Data structure of the hardware_error event.

Data Fields
uint16_t status

Result code

  • 0: success
  • Non-zero: an error has occurred