sl_bt_evt_test_dtm_completedTesting Commands

Indicates that the radio has processed a test start or end command.

Data Structures

struct  sl_bt_evt_test_dtm_completed_s
 Data structure of the dtm_completed event.
 

Macros

#define sl_bt_evt_test_dtm_completed_id   0x000e00a0
 Identifier of the dtm_completed event.
 

Detailed Description

Indicates that the radio has processed a test start or end command.

The result parameter indicates the success of the command.

After the receiver or transmitter test is stopped, the number_of_packets parameter in this event indicates the number of received or transmitted packets.


Data Structure Documentation

◆ sl_bt_evt_test_dtm_completed_s

struct sl_bt_evt_test_dtm_completed_s

Data structure of the dtm_completed event.

Data Fields
uint16_t result

Command result

uint16_t number_of_packets

Number of packets

Only valid for sl_bt_test_dtm_end command.