sl_bt_evt_user_message_to_hostUser Messaging

Used by the target application on a device to initiate communication and send a message to the NCP host.

Data Structures

struct  sl_bt_evt_user_message_to_host_s
 Data structure of the message_to_host event.
 

Macros

#define sl_bt_evt_user_message_to_host_id   0x00ff00a0
 Identifier of the message_to_host event.
 

Detailed Description

Used by the target application on a device to initiate communication and send a message to the NCP host.

Do not send event messages in the context of the user command handling.


Data Structure Documentation

◆ sl_bt_evt_user_message_to_host_s

struct sl_bt_evt_user_message_to_host_s

Data structure of the message_to_host event.

Data Fields
uint8array message

The message